Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
DC Fast-Charging Block Diagram

The first stage of the power conversion in a DC fast-charging block diagram is the high-voltage AC-to-DC conversion stage. A power factor correction (PFC) block accomplishes this AC-to-DC conversion while also increasing the power factor/power quality. Depending on the topology, various power devices as well as gate driver products are recommended, as shown here. The particular diagram at the top of this slide is a Vienna topology unidirectional PFC stage. However, part recommendations for the bidirectional topology of the various power levels are also shown.

PTM Veröffentlicht am: