Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Bidirectional DC Fast-Charging Block Diagram Image of ROHM's Bidirectional DC Fast-Charging Block Diagram

The diagram here shows a typical setup for a bidirectional DC fast-charging industrial station. It allows power flow not only for charging an EV, but also to charge back from the EVK to the electric grid. In the image, the PFC stage is shown in a 3-phase bidirectional configuration, and the DC/DC stage as a dual-active bridge (DAB) resonance isolated bidirectional converter.

PTM Veröffentlicht am: