Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Summary

In summary, when designing an electronic circuit, especially power system circuits, it is necessary to select a circuit configuration (topology) that meets the required specifications because input voltage, output voltage, power, and isolation vary depending on the application. The selection of the most suitable components also differs depending on the topology. If the wrong components are selected, the required specifications cannot be met, and the circuit design must be redone.

PTM Veröffentlicht am: