Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Unidirectional DC Fast-Charging Block Diagram Image of ROHM's Unidirectional DC Fast-Charging Block Diagram

This block diagram shows a typical setup for a unidirectional DC fast-charging industrial station. The upper portion shows the main power path: power is taken from the 3-phase AC supply line and converted from AC to DC via a power factor correction (PFC) stage before then being further converted through a high-voltage (HV) DC-to-DC converter stage. In the image, the PFC stage is shown in a Vienna rectifier configuration, and the DC/DC stage is an LLC isolated converter. The lower portion shows auxiliary and other circuitry which includes control circuits for the power stage as well as the lower power AC/DC converter and other interface-related circuitry for the display and communication buses.

PTM Veröffentlicht am: