Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
SPIRIT1 RF Transceiver Overview Slide 9

The chart on this slide illustrates the specifics of the low-power mode. The low-power mode is enabled using an internal RC oscillator of 34.7 kHz. When this mode is configured, the internal oscillator is used to periodically wake up the device in order to transmit and receive. In this case, there is very low power consumption and at the same time an efficient communication link. The wake-up period can be programmed inside the SPIRIT1, so the user can decide exactly when to wake up the device in low power mode.

PTM Veröffentlicht am: