Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
SPIRIT1 RF Transceiver Overview Slide 11

Shown on this slide is another important feature of the device, the low battery indicator. This can be programmed to tell the host microcontroller that there is a low battery level. The user can program the battery level threshold from 2.1 V to 2.7 V or they can select the brownout value with a fixed level of 1.535 V.

PTM Veröffentlicht am: