Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
SPIRIT1 RF Transceiver Overview Slide 16

In order to use the Boost mode, it is only necessary to move the supply end of L0 from one point to another. Normally L0 biases the PA with 1.4 V from the internal switch mode power supply to achieve highest efficiency, but it can be connected to the battery voltage for power output greater than 11 dBm. This function is fully documented in Application note AN4198.

PTM Veröffentlicht am: