Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
SPIRIT1 RF Transceiver Overview Slide 20

In the development kits, the evaluation board includes a daughter board which contains the SPIRIT1 chipset and a mother board with an STM32L on board (ST provides libraries and stack in order to evaluate the communication). Also included are a graphical user interface and two antennas for the communication. The daughter board has an SMA connector for connection of the antenna.

PTM Veröffentlicht am: