Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Physical Diff

Throughout the years, the CAN protocol has been adapted to specific applications and is now available in there three variants: HS-CAN (high speed), FT-CAN (fault tolerant), and SW-CAN (single wire). The FT-CAN protocol arose from a need for a fault tolerant communications network which continued to operate even if one of the wires was disconnected. Although this configuration had many advantages, its one major drawback was a reduced communication speed. In the last few years the demand for FT-CAN has declined while demand for SW-CAN and HS-CAN has increased. SW-CAN is a single wire system intended for non-critical functions.

PTM Veröffentlicht am: