Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Auto Net 2

Previously, all electronic connections were made with separate wires. Over time, the number and complexity of current automotive systems have made wire harnesses impractical. The solution was a simple 2 wire bus network. Each ECU is connected to the system bus and only responds to commands such as lights on, opening windows, or move seat forward when properly addressed. Today’s vehicles use several standard buses such as CAN, LIN and FlexRay. In order to transmit and receive commands on the bus each ECU must have dedicated transceivers. NXP provides transceivers for all the standard IVN bus protocols.

PTM Veröffentlicht am: