Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
IVN 2

There are many physical and electrical differences between the bus types. CAN is a single or two wire bus that uses 5V signal levels. It also offers several communication speeds of 40 kb/s to 125 kb/s or 1 Mb/s. LIN is a single wire bus with 12V signal levels and a maximum communication speed of 20 kb/s. FlexRay is a two wire bus system with low voltage signal levels (around 700mV), and a maximum communications speed of 10 Mb/s. This training module will discuss the CAN and LIN buses which are most commonly used in the automotive industry. FlexRay is a new protocol, still in its definition stage, which will be used for the vehicles in the next decade.

PTM Veröffentlicht am: