Maker.io main logo

CoreXY Chessboard: Electronics Meet Classic Chess

542

2025-09-24 | By Andrew Kazour

License: General Public License 3D Printing Displays LCD / TFT Magnets Microcontrollers Motors Pushbutton Stepper Switches

Chess was invented around 1500 years ago and is one of the oldest board games in existence. We decided to take a modern approach to chess with an automated chessboard and electronic-themed pieces. This chessboard can play famous chess games or just have computers battling each other all day for your enjoyment!

chessboard_1

We are using an electromagnet under the chessboard, attached to a 2-dimensional gantry, to move the pieces around. To start, we create a mechanical design for our gantry based on CoreXY kinematics. To do that, we have to understand the CoreXY gantry system. The CoreXY gantry system has both X and Y motors stationary and on the same plane. Instead of each motor controlling only one axis directly, the belts are routed in a special crossed pattern so that the movement of one motor moves the electromagnet diagonally, and the coordinated movement of both motors allows precise control of X and Y positioning. This design reduces the moving mass since the motors don’t travel with the gantry, allowing for faster and more efficient motion while maintaining accuracy.

pattern_2

CoreXY | Cartesian Motion Platform

We have to design the CoreXY gantry with extrusions, 3D prints, belts, pulleys, idlers, and a linear rail. We first have to make a square out of the extrusions, and then we use 3D printed brackets to hold it together. After that, we put on the carriages, which have 3D printed wheels with bearings inside to roll across the extrusion. These carriages are connected with a linear rail between them to allow for movement forward and backward, as well as left and right.

design_3

One major challenge we had was getting the right tension for the linear rail with the carriages. If it were too tight, then the wheels wouldn’t spin, and there would be too much friction. If it were too loose, then the linear rail would wobble and not be straight when moving, causing accuracy issues. To solve this issue, we only had wheels on the outside of the extrusion on each side and made sure they were tensioned tightly, which allowed them to move smoothly while being tensioned properly.

tension_4

Now it's time for the most important part, which is the belt setup. The belts on each of the motors go around the square using idlers and connect to the middle of the linear rail on one side. On the other side, it goes around 1 idler and connects to the middle of the linear rail. When this is all connected, we can now use the equations for moving the electromagnet where we want to go.

Now that we have a functional CoreXY gantry, it's time to make it move electronically. We will be using an XRP robotics board from SparkFun, which is equipped with a Raspberry Pi RP2350 microcontroller as the brains of the operation. The motors are 12V stepper motors driven by EasyDriver motor controllers from SparkFun. All of that is powered by a 12V power supply and a 5V buck converter. An electromagnet is hooked to the XRP using a transistor.

diagram_5

easydriver_6

Now we should keep in mind some careful circuit design considerations. The electromagnet works off 5V, but since our main power source is 12V, we use a buck converter to step it down.

circuits_7

We can’t power the electromagnet directly from the GPIO pin because it needs more current than the pin can handle, so we use an NPN transistor as a switch. The GPIO signal goes through a resistor to the base of the transistor, which allows the constant 5V from the buck converter to turn on and off for the electromagnet. A flyback diode is placed across the electromagnet to protect the transistor from negative voltage spikes when it switches off.

power_8

diagram_9

Now that we have the electronics integrated into the gantry, it's time for code! First, we will start by putting together the movement functions. We are coding the XRP board with the Arduino IDE, and we are going to be creating classes for all the movement functions to allow for easy implementation when we make it play chess.

code_10

To implement the code, we use the equations of motion for the CoreXY system from before to move the gantry how we want. Using this method, we can have the pieces move in a straight line, an L shape, and diagonally, which covers the moves on a chessboard. To get the pieces to go in between other pieces (like in the case of a knight), we have the piece move a half chessboard square to the left or right and then move around the board. This allows all the pieces to be able to move between all other pieces in any scenario.

motion_11

We need a place to put the captured pieces somewhere out of the way during the game. We will put the captured pieces on the outsides of the board, so now the 8X8 chess board becomes a 10X10. All around the board, the chess pieces are lined up when captured, which allows the board to automatically reset the game.

pieces_12

Now that we know it has to go in the 10X10 grid, we can add limit switches to the X and Y axes, so we know the boundaries of the board. The gantry will start with a homing sequence where it first moves to the X limit switch and then moves directly to the Y limit switch.

switch_13

We have the board laid out, the baseline movements needed, and a capture zone. Now we can implement the chess engine. The engine is based on the Micro-Max chess algorithm, made by Harm Muller, a program known for being computationally light, perfect for embedded processors like the XRP’s Raspberry Pi RP2350. The next step is to make the chess engine play computer vs computer games.

One specific problem we have to fix is that when the chess engine plays itself, it always plays the same game. This is because it always chooses the best move possible on both sides. To fix this issue, we need to edit the chess engine to make it randomly choose from a few moves that are all considered relatively equal. This fix allows for a unique computer vs computer game to be played each time! Note that there is a tradeoff here; although game variability has increased, the strength of the engine has slightly decreased. Throughout the coding process, we can debug by printing the board state to the serial monitor.

monitor_14

Another major problem we had was the friction on the chessboard. Each piece is made with a small hole in the bottom for a neodymium magnet, which is then covered up by some fabric. The polycarbonate on the top of the board didn't have low enough friction with the pieces, so sometimes the magnet dropped them. We spent a lot of time testing with different materials and came to the conclusion that MicroPolyester on the bottom of the piece interacted the best with the polycarbonate.

friction_15

Now that the Game code is working, we can add a UI using an LCD screen, easily connectable via the onboard Qwiic connector. We add 2 buttons to help the user navigate the UI and to add pause and reset functionalities to the board.

screen_16

The code for the LCD screen and the buttons should be relatively simple. The code is based on the SparkFun SerLCD Arduino Library, with some custom modifications. We can have a function that prints a string centered on the display. We also specify which line of the LCD we would like to have the string displayed on.

code_17

After adding the UI with the LCD and buttons, we now have a fully functioning electromagnetic chessboard!

chessboard_18

View videos

Tempo, Tactics, and Torque- Building a Robotic Chessboard Part 1

From Code to Checkmate- Building a Robotic Chessboard Part 2

If you’re interested in learning more about the full code used, here is a link to the GitHub repository

https://github.com/vincentbkrenz/DigiChess

Référence fabricant 28009
EXPERIENTIAL ROBOTICS PLATFORM (
SparkFun Electronics
101,95 €
Afficher plus Details
Référence fabricant COM-21255
EVAL BOARD FOR AP63357
SparkFun Electronics
Référence fabricant 12779
STEPPER DRIVER 0.75A 30V LOAD
SparkFun Electronics
Référence fabricant 09238
STEPPER MOTOR HYBRID BIPOLAR 12V
SparkFun Electronics
Référence fabricant TIP120
TRANS NPN DARL 60V 5A TO-220
STMicroelectronics
Référence fabricant 1N4148
DIODE STANDARD 100V 200MA DO35
onsemi
Référence fabricant 3873
5V ELECTROMAGNET 5KG HOLDING FOR
Adafruit Industries LLC
Référence fabricant SS-3GL13PT
SWITCH SNAP ACTION SPDT 3A 125V
Omron Electronics Inc-EMC Div
Référence fabricant GT2-BELT1M-6MM
GT2-BELT1M-6MM
Olimex LTD
Référence fabricant GT2-5T30-6MM
GT2-5T30-6MM
Olimex LTD
Référence fabricant 1515-72
1.5" X 1.5" T-SLOTTED EXTRUSION
80/20, LLC
Référence fabricant CF14JT10K0
RES 10K OHM 5% 1/4W AXIAL
Stackpole Electronics Inc
Référence fabricant CF14JT1K00
RES 1K OHM 5% 1/4W AXIAL
Stackpole Electronics Inc
Référence fabricant 16398
SPARKFUN 20X4 SERLCD - RGB BACKL
SparkFun Electronics
Référence fabricant 3489
SWITCH PUSH SPST-NO RED 10MA 5V
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.