Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
MEMS Gyroscopes Slide 7

ST’s MEMS gyroscopes use two equal masses that are kept oscillating so that they are always moving in opposite directions, much like a tuning fork. When this system rotates, the Coriolis forces on the two masses are always in opposite directions, and the angular movement is measured using the difference in capacitance between the two sides. When a linear acceleration is applied to the sensor, both masses move in the same direction and the differential capacitance is zero. Compared to a single mass approach, the differential nature of the tuning fork makes the system intrinsically insensitive to undesired linear acceleration or vibration.

PTM Veröffentlicht am: