Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
MEMS Gyroscopes Slide 5

Let’s quickly look at the commonly-used terms for MEMS Gyroscopes. A gyroscope can rotate in 3 axes. There are two in-plane axes called pitch and roll – the X and Y axes. The third is an out of plane axis called yaw – the Z axis. Zero rate level refers to the analog or digital sensor output value when no angular rate is applied. Sensitivity always refers to the ratio between the output and input of the sensor.

PTM Veröffentlicht am: