Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
MEMS Gyroscopes Slide 18

The general schematic shown here provides the basic guidelines to correctly use ST’s gyroscopes. Only a few external components are needed, thus simplifying board design and keeping the design compact. The two output blocks are highlighted by the green circles: an optional high-pass filter and a suggested low-pass filter further adapt the bandwidth to the application requirements. Notice how the high-pass filter uses the Vref signal as a reference. A full description of the possible configurations is provided in the product datasheet.

PTM Veröffentlicht am: