Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
MEMS Gyroscopes Slide 13

A complete understanding of the main parameters associated with MEMS gyroscopes and their representation in the datasheet is very important in order to fully exploit the advanced performances provided by these products. Zero rate level is the output of the sensor when no angular rate is applied. Temperature variation could affect the sensor output even when there is no external stimulus. ST’s gyroscope family provides one of the industry’s best Zero rate level stability over an extended temperature range of -40 to +85 degrees C. This excellent performance allows users to reduce cost and effort otherwise needed for temperature compensation.

PTM Veröffentlicht am: