Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
DC-DC Conversion Cookbook Slide 4

The operation of a voltage regulator is based on automatic control theory. A voltage regulator works by comparing the output voltage to an internal reference. The difference (the error) is amplified and the result is used to increase or decrease the output voltage, to minimize the error, in what is called a closed loop feedback circuit. The output is kept at the set value, even with variations in Vin or load.

PTM Veröffentlicht am: