Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
DC-DC Conversion Cookbook Slide 19

A special subset of linear regulators are the low drop-out regulators. The drop-out is the minimum voltage across the regulator (input to output) to maintain regulation. The classification of linear regulators based on the drop-out voltage is shown on this slide along with representative part numbers in each group. A common misconception is that if a standard regulator is changed to a low drop-out regulator, the result is to save power. That is true only provided that the input voltage is reduced accordingly, because power dissipation depends on input-output multiplied by the current and if the difference Vin-Vout stays the same, so does the power. In practice an LDO achieves low power only by allowing a lower Vin to be used for the same output voltage.

PTM Veröffentlicht am: