Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
DC-DC Conversion Cookbook Slide 23

When different ICs are used on the same application board, the need may arise to provide a start up sequence or configuration. As discussed, soft-start clamps the vref and the rails reach the nominal value at the same time this is the most common case. A power sequencing can be implemented by controlling the enable pins through the PG outputs in order to initiate the soft-start phase after the previous regulator has reached the nominal value. Finally, if the soft-start clamps the out of the error amplifier the voltage rails will reach regulation in increasing order depending on their nominal values.

PTM Veröffentlicht am: