Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
DC-DC Conversion Cookbook Slide 16

This slide shows the L6928 in operation in PWM and burst modes. Between each burst of pulses the consumption is 25 µA, reducing the average power loss. As a drawback, the frequency becomes load dependent and the output voltage has a large ripple, because the regulator turns on only when the Vout falls outside of regulation to restore the set Vout. This does not happen in PWM mode where there is a clean Vout, but a continuous switching activity increases the current consumption due to switching losses.

PTM Veröffentlicht am: