Interview with Wayne Stambaugh about KiCad Electronics Development Application – Pt. 2

Last time, Wayne shared with us some of his interests in life and his passion about electronics. He made me contemplate how far we have come in the embedded space and gave me a lot of hope for the future. For those nerds out there who think only about technology, Wayne makes you aspire to go on some golf outings or go out and at least sit on your bike for the fresh air. Wayne also brought up in our previous post that he started on the mechanical side, then became interested in the electrical. I myself remember this being the case when I was young, mostly because I didn’t understand electronics yet, and it was VERY hard to put electronics back together once you got them apart. How about the rest of you out there: where and how did you get started in electronics?

In Part 2 of this three-part series, we’ll explore with Wayne his thoughts on open source coding and teamwork.

JP (Jeremy Purcell): What drives you in the open source world?

WS (Wayne Stambaugh): The need to scratch my own itch and the desire to give back to the open source community are my prime motivators. Almost from the time I began using open source software (1996), I realized that it was a superior development model. I started hacking on KiCad when I got tired of dealing with some of the less-than-stellar EDA tools I was using at the time. I had been using open source software for quite a few years by that time and I was looking for a project where I could contribute and make a difference. KiCad seemed like a good fit. Who knew it would lead me to where I am now?

JP: What would make the open source world better?

WS: It would be useful if there was less duplication of effort, but I doubt that issue will ever completely go away since open source is still very much a scratch-your-own-itch endeavor. I could also live without some of the silly arguments and unnecessary hostility that happens from time to time. It’s always a time sink that I have yet to see produce anything of value.

JP: What’s your favorite MCU?

WS: It depends on the application. For small jobs that don’t require a lot of power, I’ve always been fond of the 8-bit Atmel products. For applications that require more power, it’s really hard to beat some of the new ARM stuff out there.

JP: What are your favorite hardware tools that you use?

WS: Way back when, any piece of HP test equipment was the gold standard. Their logic analyzers were some of the best. Probably one of the coolest pieces of hardware I’ve used was a Teredyne L210 in-circuit tester. It was an emitter-collector logic (ECL) beast with 00 cables coming out of the power supplies. Even in the mid to late ’80s, if I recall, this thing could place clock edges to less than 20pS.

JP: How important is a cohesive team when it comes to getting KiCad releases out?

WS: It is very important. You have to have buy-in from all of the lead developers so they stay on task. It’s very easy to start working on the next great feature and push off bug fixing and polishing required to get a stable release out the door. It also takes a big effort by package developers, library developers, documentation writers, and translators to get everything ready for a stable release. For a project that is as big as KiCad, it’s a far bigger task than most people realize.

In Part 1, we talked with Wayne about how he got interested in electronics and coding. In Part 3, we’ll take a deeper dive with Wayne on the actual KiCad electronics development application. Stay tuned!

Achtergrondinformatie over deze auteur

Image of Jeremy Purcell

Jeremy Purcell is de programmamanager voor digitale ontwerptools en is verantwoordelijk voor het aanwerven van toolproviders en het ontwikkelen van de strategie betreffende ontwerpactiva. In 2006 kwam hij bij DigiKey werken. Voordien was hij werkzaam als Senior Applications Engineer voor verschillende campagnes rond informatie delen met de klantenbasis en klantenbetrokkenheid binnen de activiteiten. Jeremy heeft een wetenschappelijk bachelordiploma in elektrotechniek behaald bij de North Dakota State University in Fargo, ND. Elke zomer besteedt hij enkele weken aan knutselen aan stoomtrekkers om die te laten rijden, zijn grote hobby. De rest van het jaar droomt hij van deze machines.

More posts by Jeremy Purcell
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum