A Novel Twist: Maxim Integrated Removes Risk of RISC-V with a Dual-Core Arm/RISC-V Microcontroller

While Arm cores have proven themselves reliable and are now in most mobile devices and Internet of Things (IoT) endpoints, it’s always both useful and reassuring to have an alternative, as one size does not always fit all.

Enter the RISC-V 32-bit CPU. RISC-V (pronounced risk-five) is an open-source, no royalty architecture that is the first serious competition to the entrenched Arm CPU core ecosystem in a very long time. The base RV32 variant has 31 general-purpose, 32-bit registers named x1 to x31 (register x0 is hard-wired to 0). It supports extensions to the architecture that allow flexibility for different applications. For example, when building a microcontroller, the “B” RISC-V extension supports native bit manipulation, which in my long experience with microcontrollers is an indication that the architecture is serious about the deep embedded stuff.

The challenge, however, is getting engineers to accept a new architecture. It’s always a rocky road to adoption when you go against the existing sourcing momentum.

Maxim Integrated has solved this adoption problem by going in the direction of the sourcing momentum. The MAX78000EXG+ is a dual-core microcontroller with a 100 megahertz (MHz) Arm Cortex-M4 core with a floating-point unit (FPU) and a wide variety of serial communications interfaces. However, the Arm core shares the main bus with a second, 32-bit RISC-V core (Figure 1). The second core isn’t the only reason the MAX78000EXG+ is worth a closer look. The microcontroller has a 442 kilobyte (Kbyte) weight convolutional neural network (CNN) accelerator for artificial intelligence (AI) pattern matching. The RISC-V core is mainly there to act as a programmable smart direct memory access (DMA) to move data between the CNN and on-chip memory. However, the RISC-V core can also act independently, technically making the MAX78000EXG+ a dual-core processor.

Figure 1: The Maxim Integrated MAX78000EXG+ microcontroller has an Arm Cortex-M4 core with an FPU, alongside a RISC-V core. It also has a wide variety of serial interfaces, as well as a CNN for AI processing. (Image source: Maxim Integrated)

Now, I could do a comparison of the RISC-V and Arm architecture variants and ecosystems, but the raw truth is every time an engineering team sources a new microcontroller architecture not used by their employer, they are making a career decision. For example, a module maker risks having their product rejected by an integrator because the main core used in the product is not popular, or to use a more nebulous term “industry-accepted”. I saw this happen when I was with a semiconductor company and visiting a digital camera module manufacturer.

The company had built an impressive digital camera module based on a very niche digital signal processor (DSP), and when I write “niche”, I mean I estimated it had less than 10% of the DSP market. Regardless, the digital camera module had impressive statistics, and despite my deft PowerPoint and highly developed verbal communication skills, I could not persuade the module manufacturer to use my DSP—initially.

As it turned out, the digital camera integrators the module maker approached did not share their enthusiasm for the niche DSP. Despite its clear performance advantage, no camera integrators were willing to partner with the company and buy their module. The niche DSP core with its impressive specifications was too much of an unknown, and without sufficient market adoption, there was a concern that the DSP would be discontinued. After a quick recalibration, the module maker came back to me, and we ported their code to our DSP.

Another concern with sourcing a new core is that engineers just don’t have much experience—if any—with the architecture. In this situation, they can underestimate how the core can perform in their application, or what the real memory requirements are. Unlike sourcing a voltage regulator, it can take many months of development work, including the feature creep that often finds its way into the application, before it’s discovered that the selected core underperforms.

Maxim Integrated has apparently solved the engineering and business risks associated with sourcing the RISC-V core with the MAX78000EXG+. When not used as a smart DMA, the RISC-V core can be used as a second one in the application. Any concerns about performance are easily put to rest by the comforting presence of a Cortex-M4 and its nearby FPU.

Conclusion

Sourcing a new core such as the RISC-V can be ripe with uncertainty as to its performance in an application. Suitability for purpose and memory requirements are as yet unknown, and it can take months of coding before its capabilities are fully understood and appreciated. However, the Maxim Integrated MAX78000EXG+ has made it possible, in one of engineering’s great ironies, for an Arm core to reduce the technical and business concerns of adopting the RISC-V core in a new application.

Achtergrondinformatie over deze auteur

Image of Bill Giovino

Bill Giovino is een ingenieur in elektronica met een BSEE van de Syracuse University. Hij is een van de weinigen die met succes de overstap maakten van ontwerpingenieur naar ingenieur veldtoepassingen en vervolgens naar technologiemarketing.

Meer dan 25 jaar lang heeft Bill met veel toewijding nieuwe technologieën gepromoot ten overstaan van zowel technisch als niet-technisch publiek voor vele bedrijven, waaronder STMicroelectronics, Intel en Maxim Integrated. Toen hij bij STMicroelectronics actief was, hielp Bill bij de doorbraak van de eerste successen van het bedrijf in de sector van microcontrollers. Bij Infineon stond Bill in voor de eerste toepassingen van het microcontrollerontwerp van het bedrijf in de Amerikaanse autosector. Als marketing consultant voor zijn bedrijf CPU Technologies, hielp Bill vele bedrijven om laag presterende producten op te krikken en er een succesverhaal van te maken.

Bill was een van de eersten die het Internet of Things toepaste. Hij plaatste de eerste volledige TCP/IP-stack op een microcontroller. Bill is trouw aan het motto “Verkoop via opvoeding” en wijst op het toenemende belang van duidelijke, goed geschreven mededelingen om producten online te promoten. Hij is moderator van de populaire LinkedIn Semiconductor Sales & Marketing Group en spreekt vlot B2E.

More posts by Bill Giovino
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum