Johanson Technology's 2450AT42E010xx Chip Antenna

Johanson Technology's 2450AT42E010xx Chip Antenna (Image source: Johanson Technology)

Miniature ceramic RF chip antennas are commonly used in 2.4 GHz wireless applications such as Bluetooth, WiFi, and ZigBee because they are low cost and small in physical size. Johanson Technology’s 2450AT42E010xx chip antennas have these features, but also provide another unique benefit. The antennas were specifically designed for applications where metal is directly underneath the antenna and is actually required for the antenna to perform optimally. The benefit of this characteristic is that the performance of the antenna will not be negatively affected by proximity to a coin cell battery or display containing metal. This allows smaller PCB designs and provides flexibility in the form factor and placement of the end product.

More information about this product can be found on EEWiki, and if there are any questions, feel free to ask them in the TechForum.

Achtergrondinformatie over deze auteur

Image of Scott Raeker

Scott Raeker, Principal Application Engineer bij DigiKey, is sinds 2006 in dienst en zijn voornaamste verantwoordelijkheid is het ondersteunen van klanten bij draadloze toepassingen. Hij heeft meer dan 35 jaar ervaring in de elektronische sector en is afgestudeerd in Elektrotechniek aan de Universiteit van Minnesota. Scott geniet in zijn vrije tijd van het opknappen van zijn oude boerderij.

More posts by Scott Raeker
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum