Maker.io main logo

SparkFun Temperature Sensor - STTS22H (Qwiic) Hookup Guide

116

2024-01-02 | By SparkFun Electronics

License: See Original Project

Courtesy of SparkFun

Guide by ELL C

Introduction

The SparkFun Temperature Sensor - STTS22H (Qwiic) and the SparkFun Micro Temperature ‎Sensor - STTS22H (Qwiic) are Qwiic enabled breakout boards based on the ultralow-power, high-‎accuracy, digital temperature sensor STTS22H from ST Microelectronics. Thanks to its factory ‎calibration the STTS22H offers high-end accuracy performance over the entire operating ‎temperature range, reaching as low as ±0.5 °C without requiring any further calibration at the ‎application level.‎

 

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything ‎though depending on what you have. Add it to your cart, read through the guide, and adjust the cart ‎as necessary.‎

SparkFun Temperature Sensor - STTS22H (Qwiic) Hookup Guide Wish List SparkFun ‎Wish List

VIEW SPARKFUN TEMPERATURE SENSOR - STTS22H (QWIIC) HOOKUP GUIDE WISH ‎LIST ON SPARKFUN.COM

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.‎

qwiic_1

Qwiic Connect System

We would also recommend taking a look at the following tutorials if you aren't familiar with them.‎

  • What is an Arduino?: What is this 'Arduino' thing anyway? This tutorial dives into what an ‎Arduino is and along with Arduino projects and widgets.‎

  • Installing Arduino IDE: A step-by-step guide to installing and testing the Arduino software on ‎Windows, Mac, and Linux.‎

  • How to Install FTDI Drivers: How to install drivers for the FTDI Basic on Windows, Mac OS X, ‎and Linux.‎

  • Using the Arduino Pro Mini 3.3V: This tutorial is your guide to all things Arduino Pro Mini. It ‎explains what it is, what it's not, and how to get started using it.‎

Hardware Overview

STTS22‎

The STTS22H is an ultralow-power, high-accuracy, digital temperature sensor offering high ‎performance over the entire operating temperature range. Thanks to its factory calibration the ‎STTS22H offers high-end accuracy performance over the entire operating temperature range, ‎reaching as low as ±0.5 °C without requiring any further calibration at the application level. The ‎sensor operating mode is user-configurable and allows selecting between different ODRs (down to ‎‎1 Hz) or the one-shot mode for battery saving. In one-shot mode, the sensor current consumption ‎falls to 1.75 µA. For more information, refer to the datasheet.‎

stts2

STTS22‎

stts3

STTS22 on Micro

Qwiic Connectors

There are two Qwiic connectors on either side of the SparkFun Temperature Sensor - STTS22H to ‎provide power and I2C connectivity simultaneously. The Micro version has a single Qwiic connector ‎that again provides power and I2C connectivity. The I2C address of both boards is 0x3C by default, ‎but the 1x1 board has 3 other addresses the board can be configured to use, while the Micro has 1 ‎other address available.‎

connectors_4

Qwiic Connectors

connectors_5

Qwiic Connector on Micro

Power

Ideally, power will be supplied via the Qwiic connector(s). Alternatively, power can be supplied ‎through the header along the bottom side of the board labeled 3V3 and GND. The input voltage ‎range should be between 1.5-3.6V. The Micro version has a single Ground Pin available.‎

pins_6

3.3V & GND Pins

pins_7

GND Pin on Micro

Note: There is no onboard voltage regulation on either of these boards. If you choose to provide ‎power via the plated through holes, ensure that your voltage does not exceed 5.5V.‎

Interrupt Pin

An interrupt pin is available to signal the application whenever the selectable high or low threshold ‎has been exceeded.‎

interrupt_8

Interrupt Pin

interrupt_9

Interrupt Pin on Micro

Power LED

Hopefully, this is self-explanatory, but this LED lights up when power is supplied to the board.‎

power_10

Power LED

power_11

Power LED on Micro

Exposed Pad

There's an extra pad on the bottom side of each board that allows for the most accurate possible ‎readings.‎

pad_12

Exposed Pad

pad_13

Exposed Pad on Micro

Jumpers

LED Jumper

If power consumption is an issue, cut this jumper to disable the LED on the front of the board.‎

led_14

Power LED Jumper

led_15

Power LED Jumper on Micro

Address Jumpers

The 1x1 board has two address jumpers available. The default I2C address is 0x3C. By cutting ‎various trace combinations, there are three other I2C addresses available.‎

table_16

address_17

Address Jumper

address_18

Address Jumper 1

The Micro version of this board has a single address jumper that affords the ability to change the ‎I2C address from 0x3C (Default) to 0x38.‎

micro_19

I2C Jumper

These boards are both equipped with pull-up resistors. If you are daisy chaining multiple Qwiic ‎devices, you will want to cut this jumper; if multiple sensors are connected to the bus with the pull-‎up resistors enabled, the parallel equivalent resistance will create too strong of a pull-up for the bus ‎to operate correctly. As a general rule of thumb, disable all but one pair of pull-up resistors if ‎multiple devices are connected to the bus. To disable the pull up resistors, use an X-acto knife to ‎cut the joint between the two jumper pads highlighted below.‎

jumper_20

I2C Jumper

jumper_21

I2C Jumper on Micro

Board Outline

The standard Temperature Sensor STTS22H Breakout measures 1" x 1".‎

board_22

The Micro Temperature Sensor STTS22H Breakout measures 0.75" x 0.3".‎

board_23

Hardware Hookup

The delightful thing about our Qwiic System is that it makes hooking up your project as easy as plug ‎and play. Pop one end of your Qwiic connector into the controlling board and plug the other end of ‎your Qwiic connector into your Temperature Sensor board! Voila!‎

hardware_24

hardware_25

Software Setup

Note: Make sure you are using the latest stable version of the Arduino IDE on your desktop. If this ‎is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have ‎not previously installed an Arduino library, please check out our installation guide.‎

SparkFun has written a library to work with the SparkFun Temperature Sensor - STTS22H (Qwiic). ‎You can obtain this library through the Arduino Library Manager by searching for "STTS22H". Find ‎the one written by SparkFun Electronics and install the latest version. If you prefer downloading ‎libraries manually, you can grab them from the GitHub Repository.‎

SPARKFUN STTS22H ARDUINO LIBRARY GITHUB

Examples

Example 1: Basic

Now that we've got our library installed and our hardware all hooked up, let's look at some examples.‎

This first example just does some basic measurements. To find Example 1, go ‎to File > Examples > SparkFun Temperature Sensor - STTS22H > example1-basic:‎

basic_26

Or alternatively you can copy and paste the code below into a nice shiny new Arduino window:‎

Copy Code
/*
example1-basic.ino

This example shows basic data retrieval from the SparkFun Temperature Sensor - STTS22H.

Output Data Rates: 

STTS22H_POWER_DOWN
STTS22H_ONE_SHOT  
STTS22H_1Hz       
STTS22H_25Hz      
STTS22H_50Hz      
STTS22H_100Hz     
STTS22H_200Hz     

Written by: 
Elias Santistevan @ SparkFun Electronics December, 2022

Products: 
   SparkFun Temperature Sensor - STTS2H              https://www.sparkfun.com/products/21262
   SparkFun Micro Temperature Sensor - STTS2H        https://www.sparkfun.com/products/21051

Repository:
     https://github.com/sparkfun/SparkFun_STTS22H_Arduino_Library

SparkFun code, firmware, and software is released under the MIT
License(http://opensource.org/licenses/MIT).

*/

#include <Wire.h>
#include "SparkFun_STTS22H.h"

SparkFun_STTS22H mySTTS; 

float temp; 

void setup()
{

    Wire.begin();

    Serial.begin(115200);

    if( !mySTTS.begin() )
    {
        Serial.println("Did not begin.");
        while(1);
    }

    Serial.println("Ready");

    // Other output data rates can be found in the description
    // above. To change the ODR or mode, the device must first be
    // powered down.
    mySTTS.setDataRate(STTS22H_POWER_DOWN);
    delay(10);
    mySTTS.setDataRate(STTS22H_1Hz);

    // Enables incrementing register behavior for the IC.
    // It is not enabled by default as the datsheet states and
    // is vital for reading the two temperature registers.
    mySTTS.enableAutoIncrement();

    delay(100);
}

void loop()
{

    // Only use data ready for one-shot mode or 1Hz output. 
    if( mySTTS.dataReady() ) 
    {

        mySTTS.getTemperatureF(&temp);

        // Temperature in different units can be retrieved
        // using the following functions.

        //mySTTS.getTemperatureC(&temp);
        //mySTTS.getTemperatureK(&temp);

        Serial.print("Temp: "); 
        Serial.print(temp);
        Serial.println("F"); 

    } 

    // delay = 1/ODR 
    delay(1000);

}

Once you're ready to go, go ahead and hit the upload button (the right facing arrow button under ‎the "Edit" menu item). Once your code is uploaded, open the Serial Monitor and you'll see ‎information start printing out.‎

upload_27

Example 2: Interrupt

Example 2 can be found under File > Examples > SparkFun Temperature Sensor - ‎STTS22H > example2-interrupt:‎

example_28

You can also copy the code below into a new Arduino file:‎

Copy Code
/*
example2_basic.ino

This example desmonstrates how to set temperature thresholds to trigger an interrupt. 

Output Data Rates: 

STTS22H_POWER_DOWN
STTS22H_ONE_SHOT  
STTS22H_1Hz       
STTS22H_25Hz      
STTS22H_50Hz      
STTS22H_100Hz     
STTS22H_200Hz     

Written by: 
Elias Santistevan @ SparkFun Electronics December, 2022

Products: 
   SparkFun Temperature Sensor - STTS2H              https://www.sparkfun.com/products/21262
   SparkFun Micro Temperature Sensor - STTS2H        https://www.sparkfun.com/products/21051

Repository:
     https://github.com/sparkfun/SparkFun_STTS22H_Arduino_Library

SparkFun code, firmware, and software is released under the MIT
License(http://opensource.org/licenses/MIT).

*/

#include <Wire.h>
#include "SparkFun_STTS22H.h"

SparkFun_STTS22H mySTTS; 

float temp; 

// These values are in Farenheit
float interruptHighValue = 90.5;
float interruptLowValue = 42.0;

int tempInterrupt = 2; 

void setup()
{

    Wire.begin();

    Serial.begin(115200);

    pinMode(tempInterrupt, INPUT);

    if( !mySTTS.begin() )
    {
        Serial.println("Did not begin.");
        while(1);
    }

    Serial.println("Ready");

    // Other output data rates can be found in the description
    // above. To change the ODR or mode, the device must first be
    // powered down.
    mySTTS.setDataRate(STTS22H_POWER_DOWN);
    delay(10);
    mySTTS.setDataRate(STTS22H_25Hz);

    // Enables incrementing register behavior for the IC.
    // It is not enabled by default as the datsheet states and
    // is vital for reading the two temperature registers.
    mySTTS.enableAutoIncrement();


    // Set interrupts for both lower and higher thresholds.
    // Note: These functions accept Farenheit as their arguments.
    // Other functions for different units just below. 
    mySTTS.setInterruptLowF(interruptLowValue);
    mySTTS.setInterruptHighF(interruptHighValue);

    //mySTTS.setInterruptLowC(interruptLowValue);
    //mySTTS.setInterruptHighC(interruptHighValue);

    //mySTTS.setInterruptLowK(interruptLowValue);
    //mySTTS.setInterruptHighK(interruptHighValue);

    delay(100);
}

void loop()
{

    // Checking if data ready is not necessary when output is set higher 
    // than 1Hz. 
    mySTTS.getTemperatureF(&temp);

    // Temperature in different units can be retrieved
    // using the following functions.

    //mySTTS.getTemperatureC(&temp);
    //mySTTS.getTemperatureK(&temp);

    Serial.print("Temp: "); 
    Serial.print(temp);
    Serial.println("F"); 

    if( digitalRead(tempInterrupt) == LOW )
    {
        Serial.println("Temperature threshold"); 
        while(1);
    }

    // delay = 1/ODR 
    delay(1000);

}

Note that depending on which processor board you are using, you may need to alter the Interrupt ‎Pin. Since we're using a RedBoard here, our Interrupt Pin is 2 (int tempInterrupt = 2;). Also, in ‎this example, we've used an IC hook with a pigtail to connect the Interrupt Pin to the RedBoard pin ‎‎2, but you can also solder headers to the STTS22H Temperature Sensor so you can use the ‎interrupt pin. Your hardware hookup should look something like the following:‎

redboard_29

Once you're ready to go, go ahead and hit the upload button (the right facing arrow button under ‎the "Edit" menu item). Once your code is uploaded, open the Serial Monitor and you'll see ‎information start printing out.‎

If you have a look at the code, you'll notice that we've set our upper threshhold to 90.5 degrees F, ‎and our lower threshhold to 42 degrees F. I held the sensor in front of a heater to hit the upper ‎threshhold:‎

code_30

The lower threshhold was reached by sticking the sensor in a plastic bag and then putting that ‎plastic bag into ice water:‎

threshold_31

Example 3: One Shot

In Example 3, we're going to have a look at the One-Shot functionality. To find Example 3, go ‎to File > Examples > SparkFun Temperature Sensor - STTS22H > example3-one_shot:‎

shot_32

Or you can copy and paste the code below into a clean Arduino sketch:‎

Copy Code
/*
example3-one_shot.ino

This example shows basic data retrieval using the "one-shot" feature i.e. - get the temp
now feature. 

Output Data Rates: 

STTS22H_POWER_DOWN
STTS22H_ONE_SHOT   < -------- This one. 
STTS22H_1Hz       
STTS22H_25Hz      
STTS22H_50Hz      
STTS22H_100Hz     
STTS22H_200Hz     

Written by: 
Elias Santistevan @ SparkFun Electronics December, 2022

Products: 
   SparkFun Temperature Sensor - STTS2H              https://www.sparkfun.com/products/21262
   SparkFun Micro Temperature Sensor - STTS2H        https://www.sparkfun.com/products/21051

Repository:
     https://github.com/sparkfun/SparkFun_STTS22H_Arduino_Library

SparkFun code, firmware, and software is released under the MIT
License(http://opensource.org/licenses/MIT).

*/

#include <Wire.h>
#include "SparkFun_STTS22H.h"

SparkFun_STTS22H mySTTS; 

float temp; 

void setup()
{

    Wire.begin();

    Serial.begin(115200);

    if( !mySTTS.begin() )
    {
        Serial.println("Did not begin.");
        while(1);
    }

    Serial.println("Ready");

    // Other output data rates can be found in the description
    // above. To change the ODR or mode, the device must first be
    // powered down.
    mySTTS.setDataRate(STTS22H_POWER_DOWN);
    delay(10);
    // Force new reading, temp sensor will power down after conversion. 
    mySTTS.setDataRate(STTS22H_ONE_SHOT); 

    // Enables incrementing register behavior for the IC.
    // It is not enabled by default as the datsheet states and
    // is vital for reading the two temperature registers.
    mySTTS.enableAutoIncrement();

    delay(100);
}

void loop()
{

    // Temp sensor will power down automatically after single read.
    if( mySTTS.dataReady() ) 
    {

        mySTTS.getTemperatureF(&temp);

        // Temperature in different units can be retrieved
        // using the following functions.

        //mySTTS.getTemperatureC(&temp);
        //mySTTS.getTemperatureK(&temp);

        Serial.print("Temp: "); 
        Serial.print(temp);
        Serial.println("F"); 

        // Wait 10 seconds for until we initiate another read.
        delay(10000);

        // Enable another reading.
        mySTTS.setDataRate(STTS22H_ONE_SHOT); 

    } 

    // Demonstrative delay. 
    delay(100);

}

Once you're ready to go, go ahead and hit the upload button (the right facing arrow button under ‎the "Edit" menu item). Once your code is uploaded, open the Serial Monitor and you'll see ‎information start printing out.‎

com_33

This really isn't all that exciting until you measure the current consumption!‎

Troubleshooting

Not working as expected and need help? ‎

If you need technical assistance and more information on a product that is not working as you ‎expected, we recommend heading on over to the SparkFun Technical Assistance page for some ‎initial troubleshooting.

SPARKFUN TECHNICAL ASSISTANCE PAGE‎ ‎

If you don't find what you need there, the SparkFun Forums are a great place to find and ask for ‎help. If this is your first visit, you'll need to create a Forum Account to search product forums and ‎post questions.

CREATE NEW FORUM ACCOUNT     LOG INTO SPARKFUN FORUMS

Resources and Going Further

SparkFun Temperature Sensor - STTS22H (Qwiic):

‎SparkFun Micro Temperature Sensor - STTS22H (Qwiic):

‎General Information:

Référence fabricant 21262
SPARKFUN TEMPERATURE SENSOR - ST
SparkFun Electronics
Référence fabricant 21273
SPARKFUN MICRO TEMPERATURE SENSO
SparkFun Electronics
Référence fabricant 15123
REDBOARD QWIIC ATMEGA328 EVAL BD
SparkFun Electronics
Référence fabricant 14427
QWIIC CABLE - 100MM
SparkFun Electronics
Référence fabricant 09741
TEST LEAD HOOK TO TIP PLUG 2.5"
SparkFun Electronics
Référence fabricant 15428
CBL USB2.0 A PLG-MCR B PLG 2.62'
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.