Maker.io main logo

QR Code Detection Using OpenCV Based on UNIHIKER

220

2025-08-14 | By DFRobot

License: Attribution Arduino ESP32

Introduction

This project aims to implement QR Code detection on UNIHIKER using OpenCV. This project interfaces a USB camera with UNIHIKER to detect QR codes in real-time using the camera and displays the decoded results on screen.

 

Project Objectives

Learn how to decode QR Codes using OpenCV and the pyzbar Library

HARDWARE LIST

1UNIHIKER - IoT Python Single Board Computer with Touchscreen

1Type-C&Micro 2-in-1 USB Cable

1USB camera

Software

- Mind+ Programming Software

 

Practical Process

1. Hardware Setup

Connect the camera to the USB port of UNIHIKER.

 

connect the camera

 

Connect the UNIHIKER board to the computer via USB cable.

 

connect to the computer

 

2. Software Development

Step 1: Open Mind+, and remotely connect to UNIHIKER.

 

connect mind+  to the unihiker

 

Step 2: Create a new file named "main.py" in "Files in Project".

 

creat a new file

 

Step 3: Write Program

Double-click to open the "main.py" file.

Sample Program:

CODE

Copy Code
import cv2  

import time

import numpy as np

from pyzbar.pyzbar import decode

def main():

    cap = cv2.VideoCapture(0)

while not cap.isOpened():

continue

    cap_w, cap_h = 240, 320

    cv2.namedWindow("qrwindows", cv2.WND_PROP_FULLSCREEN)

    cv2.setWindowProperty("qrwindows",cv2.WND_PROP_FULLSCREEN, cv2.WINDOW_FULLSCREEN)

while True:

        qrimg_success, qrimg_src = cap.read()

        xmin, ymin, w, h = 250, 100, cap_w, cap_h

        qrimg_src = qrimg_src[ymin:ymin+h, xmin:xmin+w]

        qrcode_val = decode(qrimg_src)

if len(qrcode_val) > 0:

for i in range(len(qrcode_val)):

                qrcode_str = qrcode_val[i][0].decode()

                print(qrcode_str)

                point_x = qrcode_val[i][2][0]

                point_y = qrcode_val[i][2][1]

                point_w = qrcode_val[i][2][2]

                point_h = qrcode_val[i][2][3]

                point_1_x = qrcode_val[i][3][0][0]

                point_1_y = qrcode_val[i][3][0][1]

                point_2_x = qrcode_val[i][3][1][0]

                point_2_y = qrcode_val[i][3][1][1]

                point_3_x = qrcode_val[i][3][2][0]

                point_3_y = qrcode_val[i][3][2][1]

                point_4_x = qrcode_val[i][3][3][0]

                point_4_y = qrcode_val[i][3][3][1]

                cv2.rectangle(qrimg_src, (point_x, point_y), (point_x+point_w, point_y+point_h), (255, 0, 255), 2)

                cv2.line(qrimg_src, (point_1_x, point_1_y), (point_2_x, point_2_y), (255, 0, 0), 2, cv2.FILLED)

                cv2.line(qrimg_src, (point_2_x, point_2_y), (point_3_x, point_3_y), (255, 0, 0), 2, cv2.FILLED)

                cv2.line(qrimg_src, (point_3_x, point_3_y), (point_4_x, point_4_y), (255, 0, 0), 2, cv2.FILLED)

                cv2.line(qrimg_src, (point_4_x, point_4_y), (point_1_x, point_1_y), (255, 0, 0), 2, cv2.FILLED)

                cv2.circle(qrimg_src, (point_1_x, point_1_y), 5, (255, 0, 0), 2)

                cv2.circle(qrimg_src, (point_2_x, point_2_y), 5, (0, 255, 0), 2)

                cv2.circle(qrimg_src, (point_3_x, point_3_y), 5, (0, 0, 255), 2)

                cv2.circle(qrimg_src, (point_4_x, point_4_y), 5, (255, 255, 0), 2)

                cv2.putText(qrimg_src,qrcode_str,(point_x,point_y-15), cv2.FONT_HERSHEY_COMPLEX, 0.4, (0, 0, 255), 1)

            cv2.imshow('qrwindows', qrimg_src)

            cv2.waitKey(10)

            time.sleep(1)

else:

            cv2.imshow('qrwindows', qrimg_src)

            cv2.waitKey(10)

if __name__ == '__main__':

    main()

3. Run and Debug

Run the Main Program, move the QR code into the camera's view. The screen of the UNIHIKER will display a QR code detection frame and its decoded content.

 

display a QR code

 

4. Program Analysis

In the above "main.py" file, we use the OpenCV library to access the camera and obtain real-time video streams. We then use the decode method from the pyzbar library to detect and parse strings represented by QR codes. Subsequently, we retrieve the coordinates of recognized QR codes, draw recognition boxes, and display the recognized content in real-time. The overall flow is as follows:

1. Camera Initialization:
  - Initialize the camera using cv2.VideoCapture(0), where the parameter 0 denotes the default camera device.
  - Wait for the camera to start: Use cap.isOpened() to verify if the camera has successfully opened. If not, continue waiting.

2. Create Display Window:
  - Create a window named qrwindows using cv2.namedWindow and set it to full-screen display mode.

3. Main Loop:
  - Enter an infinite loop to continuously capture images from the camera and process them for QR code detection.
  - Read image: Use cap.read() to capture a frame from the camera.
  - Cropping: Crop a region from the captured image based on predefined coordinates and size (adjusted for screen dimensions) for QR code detection.
  - Decode QR code: Apply the decode function to decode QR codes within the cropped image area.
  - Process detection results:
      - If a QR code is detected, iterate through all detected QR codes.
      - For each QR code, parse its content and print it to the console.
      - Calculate the coordinates of QR code positioning points and draw recognition boxes, connecting lines, and positioning points on the image.
      - Display the decoded QR code text above the recognition box and pause for viewing.
      - If no QR code is detected, display the camera image and continue with the next cycle.

Knowledge Corner - QR code and QR code scanning & processing

 

QR codes are a fast and convenient way to transmit information, widely used in our daily lives. For example, people can make payments to merchants without cash by scanning QR codes; consumers can scan QR codes on products to obtain detailed information and trace the origin of goods. In practice, the various uses of QR codes rely on encoding and decoding information. QR codes store encoded information, which is captured by device cameras such as smartphones when scanned. The device then decodes the QR code, ultimately restoring the encoded information to its original form.

 

QR CODE

 

A QR code consists of a matrix of black and white squares, which are recognized and decoded by scanning devices. When identifying a QR code, the process includes image acquisition and preprocessing, positioning, segmentation, decoding, and parsing, as illustrated below.

 

Illustration of the process

Project.zip168KB

Référence fabricant DFR0706-EN
UNIHIKER IOT PROGRAMMING SBC
DFRobot
Référence fabricant FIT0668
CBL A PLUG-C PLUG W/MCR B 3.28'
DFRobot
Référence fabricant FIT0701
USB CAMERA FOR RASPBERRY PI AND
DFRobot
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.