Maker.io main logo

How to Perform Object Detection with TensorFlow Lite on Raspberry Pi

1.504

2020-10-19 | By ShawnHymel

License: Attribution Raspberry Pi SBC

Object detection is a difficult problem in the field of computer vision. It requires computers to look at an image (or individual frame from a video stream), identify any objects of interest, and then classify each object. This technique is useful for tracking people at a crosswalk, tracking faces for facial recognition, looking for obstacles in a self-driving car, and helping robots identify objects it can manipulate.

In this tutorial, I’ll walk you through the process of installing TensorFlow Lite on a Raspberry Pi and using it to perform object detection with a pre-trained Single Shot MultiBox Detector (SSD) model.

You can watch this tutorial in video form here:

 

Required Hardware

You will need the following hardware to complete this tutorial:

Prepare Raspberry Pi

For this tutorial, you can use a Raspberry Pi 3B+ or Raspberry Pi 4 (4 or 8 GB model). While either will work, object detection runs much faster on the Pi 4, as it has a faster processor and more memory. In my experience, the TensorFlow Lite (TFLite) model used in this tutorial will give you about 1 frame per second (fps) on the Pi 3 and about 5 fps on the Pi 4.

Raspberry Pi 3 and Raspberry Pi 4

Connect a Raspberry Pi camera to the Raspberry Pi’s camera slot (ZIF connector in the middle of the board). Note that I used a Pi camera V2 for this demo, but a V1 camera or USB webcam should also work.

Raspberry Pi Camera Module V2

Follow this guide to install the latest version of Raspbian onto a microSD card. When you boot the Pi, go through the steps to configure the operating system (use the command raspi-config if you do not get an initial pop-up window). Specifically, you will want the following:

  • Change the default password

  • Keyboard and language set to your region

  • Internet connection

  • Enable camera interface (if you’re using the Pi camera)

  • (Optional) enable SSH and VNC if you want to work on your Pi remotely

See this guide on using raspi-config.

Install TensorFlow Lite

Open a new terminal. As Raspbian defaults to Python 2 (at the time of this tutorial’s writing) and we need to use Python 3, I like to set the commands python and pip to use version 3 by default. To do that, open a new terminal and edit .bashrc:

Copy Code
cd ~
nano .bashrc

At the bottom of that document, add the following lines:

Copy Code
alias python=python3
alias pip=pip3

Adding python and pip aliases to bashrc

Save and exit the document (ctrl-x). Force a reload using the source command so you don’t need to reload the terminal:

Copy Code
source .bashrc

Let’s create a virtual environment so we can keep installed libraries and packages separate from our main terminal environment. TensorFlow can require very specific versions of libraries, so a virtual environment helps to keep things separate from the rest of your development work. We’ll do that by installing virtualenv and creating a tflite environment in our project directory. Enter the following:

Copy Code
mkdir -p Projects/Python/tflite
cd Projects/Python/tflite
python -m pip install virtualenv
python -m venv tflite-env

Now, we should have a virtual environment created in our tflite directory. Each time we wish to execute a TensorFlow Lite program, we must first activate the tflite-env virtual environment, as that’s where all of our packages and libraries are stored. To do that, run the activate script in our environment’s directory with:

Copy Code
source tflite-env/bin/activate

Your prompt should change to have a (tflite-env) preceding the directory listing. This will let you know that you are working in a virtual environment.

Using virtual environment

In this new virtual environment, install the following libraries, which assist OpenCV in processing images/videos:

Copy Code
sudo apt -y install libjpeg-dev libtiff5-dev libjasper-dev libpng12-dev libavcodec-dev libavformat-dev libswscale-dev libv4l-dev libxvidcore-dev libx264-dev

Next, we need to install a few libraries to help with the OpenCV and TensorFlow Lite backend and GUI processing:

Copy Code
sudo apt -y install qt4-dev-tools libatlas-base-dev libhdf5-103 

When those libraries have finished installing, use pip to install OpenCV. Specifically, we want v4.1.0.25, as that seems to work best for now:

Copy Code
python -m pip install opencv-contrib-python==4.1.0.25

Then, enter the following to figure out what type of processor you have and which version of Python you are using:

Copy Code
uname -m
python --version

On a Raspberry Pi 3 or 4, you should see something telling us the CPU is an “armv7l.” For me, Python is version 3.7. 

Checking uname and Python version

“armv7l” is a 32-bit ARM processor, which we’ll need to know for the next part. At the time of this writing, TensorFlow Lite will work with Python versions 3.5-3.8. If you do not have one of these versions, follow these instructions to install a different version of Python in your virtual environment.

Open an Internet browser on your Pi and head to tensorflow.org/lite/guide/python. Scroll down to the list of wheel (.whl) files and find the group that matches your OS/processor, which should be “Linux (ARM 32).” In that group, find the link that corresponds to your version of Python (3.7 for me). Right-click and select “Copy link address.”

Copying TensorFlow Lite whl file link

Back in the terminal, enter the following:

Copy Code
python -m pip install <paste in .whl link>

Paste in the link and press ‘enter.’ This should install TensorFlow Lite in your virtual environment. Note that for this tutorial, I installed TensorFlow Lite v2.1. This will take some time to install.

Installing TensorFlow Lite with pip

Download Pre-Trained Model

Training a machine learning model from scratch can be a time-consuming process. We will cover training a model for object detection in a future tutorial. For now, let’s start with a simple model that has been trained for us on the COCO dataset.

Common Objects in Context (COCO) is a large collection of images that have been tagged and labeled by researchers at Microsoft, Facebook, and a variety of universities. It contains over 200,000 images with around 90 object categories.

Object detection or object classification models can be trained on the COCO dataset to give us a starting point for recognizing everyday objects, such as people, cars, bicycles, cups, scissors, dogs, cats, and so on. We will use a MobileNet V1 model that has been trained on the COCO dataset as our object detection model.

On your Raspberry Pi, head to https://www.tensorflow.org/lite/models/object_detection/overview and download the Starter model and labels zip file. Note that if the link on that site does not work, you can download the same zip file here:

Download Starter Model and Labels

In a terminal, let’s move the .zip file to a working directory for our project and unzip it:

Copy Code
mkdir -p ~/Projects/Python/tflite/object_detection/coco_ssd_mobilenet_v1
cd ~/Projects/Python/tflite/object_detection
mv ~/Downloads/coco_ssd_mobilenet_v1_1.0_quant_2018_06_29.zip .
unzip coco_ssd_mobilenet_v1_1.0_quant_2018_06_29.zip -d coco_ssd_mobilenet_v1

You should see two files in the coco_ssd_mobilenet_v1 directory: detect.tflite and labelmap.txt. The .tflite file is our model. You can use a program like Netron to view the neural network. Notice that the input of the model is a 300x300x3 array (or, more accurately, a “tensor”). 

Viewing MobileNet with Netron

The labelmap.txt file contains an ordered list of all the possible categories. These line up with the COCO categories that were used to train the accompanying MobileNet model.

Run Object Detection

GitHub user EdjeElectronics has a great Python program for object detection that we will use as a starting point. You can view the original program here: TFLite_detection_webcam.py.

The program captures a frame from the camera using OpenCV, resizes the frame to 300x300 pixels (note that aspect ratio is not maintained), and passes the resulting tensor to TensorFlow Lite. The invoke() function returns with a list of detected objects in the frame, a confidence score of each object, and coordinates for their bounding boxes. The program takes these coordinates and draws a green rectangle around the object before displaying it to the user.

We are going to make a few additions. First, we will use cv2.WINDOW_NORMAL to create a window that can be resized. Second, we will add a section that computes the center of each object and lists detected objects to the console.

In a new text editor, paste the following code, which is EdjeElectronics' original program with our additions:

Copy Code
######## Webcam Object Detection Using Tensorflow-trained Classifier #########
#
# Author: Evan Juras
# Date: 10/27/19
# Description: 
# This program uses a TensorFlow Lite model to perform object detection on a live webcam
# feed. It draws boxes and scores around the objects of interest in each frame from the
# webcam. To improve FPS, the webcam object runs in a separate thread from the main program.
# This script will work with either a Picamera or regular USB webcam.
#
# This code is based off the TensorFlow Lite image classification example at:
# https://github.com/tensorflow/tensorflow/blob/master/tensorflow/lite/examples/python/label_image.py
#
# I added my own method of drawing boxes and labels using OpenCV.
# 
# Modified by: Shawn Hymel
# Date: 09/22/20
# Description:
# Added ability to resize cv2 window and added center dot coordinates of each detected object.
# Objects and center coordinates are printed to console.

# Import packages
import os
import argparse
import cv2
import numpy as np
import sys
import time
from threading import Thread
import importlib.util

# Define VideoStream class to handle streaming of video from webcam in separate processing thread
# Source - Adrian Rosebrock, PyImageSearch: https://www.pyimagesearch.com/2015/12/28/increasing-raspberry-pi-fps-with-python-and-opencv/
class VideoStream:
    """Camera object that controls video streaming from the Picamera"""
    def __init__(self,resolution=(640,480),framerate=30):
        # Initialize the PiCamera and the camera image stream
        self.stream = cv2.VideoCapture(0)
        ret = self.stream.set(cv2.CAP_PROP_FOURCC, cv2.VideoWriter_fourcc(*'MJPG'))
        ret = self.stream.set(3,resolution[0])
        ret = self.stream.set(4,resolution[1])
            
        # Read first frame from the stream
        (self.grabbed, self.frame) = self.stream.read()

	# Variable to control when the camera is stopped
        self.stopped = False

    def start(self):
	# Start the thread that reads frames from the video stream
        Thread(target=self.update,args=()).start()
        return self

    def update(self):
        # Keep looping indefinitely until the thread is stopped
        while True:
            # If the camera is stopped, stop the thread
            if self.stopped:
                # Close camera resources
                self.stream.release()
                return

            # Otherwise, grab the next frame from the stream
            (self.grabbed, self.frame) = self.stream.read()

    def read(self):
	# Return the most recent frame
        return self.frame

    def stop(self):
	# Indicate that the camera and thread should be stopped
        self.stopped = True

# Define and parse input arguments
parser = argparse.ArgumentParser()
parser.add_argument('--modeldir', help='Folder the .tflite file is located in',
                    required=True)
parser.add_argument('--graph', help='Name of the .tflite file, if different than detect.tflite',
                    default='detect.tflite')
parser.add_argument('--labels', help='Name of the labelmap file, if different than labelmap.txt',
                    default='labelmap.txt')
parser.add_argument('--threshold', help='Minimum confidence threshold for displaying detected objects',
                    default=0.5)
parser.add_argument('--resolution', help='Desired webcam resolution in WxH. If the webcam does not support the resolution entered, errors may occur.',
                    default='1280x720')
parser.add_argument('--edgetpu', help='Use Coral Edge TPU Accelerator to speed up detection',
                    action='store_true')

args = parser.parse_args()

MODEL_NAME = args.modeldir
GRAPH_NAME = args.graph
LABELMAP_NAME = args.labels
min_conf_threshold = float(args.threshold)
resW, resH = args.resolution.split('x')
imW, imH = int(resW), int(resH)
use_TPU = args.edgetpu

# Import TensorFlow libraries
# If tflite_runtime is installed, import interpreter from tflite_runtime, else import from regular tensorflow
# If using Coral Edge TPU, import the load_delegate library
pkg = importlib.util.find_spec('tflite_runtime')
if pkg:
    from tflite_runtime.interpreter import Interpreter
    if use_TPU:
        from tflite_runtime.interpreter import load_delegate
else:
    from tensorflow.lite.python.interpreter import Interpreter
    if use_TPU:
        from tensorflow.lite.python.interpreter import load_delegate

# If using Edge TPU, assign filename for Edge TPU model
if use_TPU:
    # If user has specified the name of the .tflite file, use that name, otherwise use default 'edgetpu.tflite'
    if (GRAPH_NAME == 'detect.tflite'):
        GRAPH_NAME = 'edgetpu.tflite'       

# Get path to current working directory
CWD_PATH = os.getcwd()

# Path to .tflite file, which contains the model that is used for object detection
PATH_TO_CKPT = os.path.join(CWD_PATH,MODEL_NAME,GRAPH_NAME)

# Path to label map file
PATH_TO_LABELS = os.path.join(CWD_PATH,MODEL_NAME,LABELMAP_NAME)

# Load the label map
with open(PATH_TO_LABELS, 'r') as f:
    labels = [line.strip() for line in f.readlines()]

# Have to do a weird fix for label map if using the COCO "starter model" from
# https://www.tensorflow.org/lite/models/object_detection/overview
# First label is '???', which has to be removed.
if labels[0] == '???':
    del(labels[0])

# Load the Tensorflow Lite model.
# If using Edge TPU, use special load_delegate argument
if use_TPU:
    interpreter = Interpreter(model_path=PATH_TO_CKPT,
                              experimental_delegates=[load_delegate('libedgetpu.so.1.0')])
    print(PATH_TO_CKPT)
else:
    interpreter = Interpreter(model_path=PATH_TO_CKPT)

interpreter.allocate_tensors()

# Get model details
input_details = interpreter.get_input_details()
output_details = interpreter.get_output_details()
height = input_details[0]['shape'][1]
width = input_details[0]['shape'][2]

floating_model = (input_details[0]['dtype'] == np.float32)

input_mean = 127.5
input_std = 127.5

# Initialize frame rate calculation
frame_rate_calc = 1
freq = cv2.getTickFrequency()

# Initialize video stream
videostream = VideoStream(resolution=(imW,imH),framerate=30).start()
time.sleep(1)

# Create window
cv2.namedWindow('Object detector', cv2.WINDOW_NORMAL)

#for frame1 in camera.capture_continuous(rawCapture, format="bgr",use_video_port=True):
while True:

    # Start timer (for calculating frame rate)
    t1 = cv2.getTickCount()

    # Grab frame from video stream
    frame1 = videostream.read()

    # Acquire frame and resize to expected shape [1xHxWx3]
    frame = frame1.copy()
    frame_rgb = cv2.cvtColor(frame, cv2.COLOR_BGR2RGB)
    frame_resized = cv2.resize(frame_rgb, (width, height))
    input_data = np.expand_dims(frame_resized, axis=0)

    # Normalize pixel values if using a floating model (i.e. if model is non-quantized)
    if floating_model:
        input_data = (np.float32(input_data) - input_mean) / input_std

    # Perform the actual detection by running the model with the image as input
    interpreter.set_tensor(input_details[0]['index'],input_data)
    interpreter.invoke()

    # Retrieve detection results
    boxes = interpreter.get_tensor(output_details[0]['index'])[0] # Bounding box coordinates of detected objects
    classes = interpreter.get_tensor(output_details[1]['index'])[0] # Class index of detected objects
    scores = interpreter.get_tensor(output_details[2]['index'])[0] # Confidence of detected objects
    #num = interpreter.get_tensor(output_details[3]['index'])[0]  # Total number of detected objects (inaccurate and not needed)

    # Loop over all detections and draw detection box if confidence is above minimum threshold
    for i in range(len(scores)):
        if ((scores[i] > min_conf_threshold) and (scores[i] <= 1.0)):

            # Get bounding box coordinates and draw box
            # Interpreter can return coordinates that are outside of image dimensions, need to force them to be within image using max() and min()
            ymin = int(max(1,(boxes[i][0] * imH)))
            xmin = int(max(1,(boxes[i][1] * imW)))
            ymax = int(min(imH,(boxes[i][2] * imH)))
            xmax = int(min(imW,(boxes[i][3] * imW)))
            
            cv2.rectangle(frame, (xmin,ymin), (xmax,ymax), (10, 255, 0), 2)
            
            # Draw label
            object_name = labels[int(classes[i])] # Look up object name from "labels" array using class index
            label = '%s: %d%%' % (object_name, int(scores[i]*100)) # Example: 'person: 72%'
            labelSize, baseLine = cv2.getTextSize(label, cv2.FONT_HERSHEY_SIMPLEX, 0.7, 2) # Get font size
            label_ymin = max(ymin, labelSize[1] + 10) # Make sure not to draw label too close to top of window
            cv2.rectangle(frame, (xmin, label_ymin-labelSize[1]-10), (xmin+labelSize[0], label_ymin+baseLine-10), (255, 255, 255), cv2.FILLED) # Draw white box to put label text in
            cv2.putText(frame, label, (xmin, label_ymin-7), cv2.FONT_HERSHEY_SIMPLEX, 0.7, (0, 0, 0), 2) # Draw label text

            # Draw circle in center
            xcenter = xmin + (int(round((xmax - xmin) / 2)))
            ycenter = ymin + (int(round((ymax - ymin) / 2)))
            cv2.circle(frame, (xcenter, ycenter), 5, (0,0,255), thickness=-1)

            # Print info
            print('Object ' + str(i) + ': ' + object_name + ' at (' + str(xcenter) + ', ' + str(ycenter) + ')')

    # Draw framerate in corner of frame
    cv2.putText(frame,'FPS: {0:.2f}'.format(frame_rate_calc),(30,50),cv2.FONT_HERSHEY_SIMPLEX,1,(255,255,0),2,cv2.LINE_AA)

    # All the results have been drawn on the frame, so it's time to display it.
    cv2.imshow('Object detector', frame)

    # Calculate framerate
    t2 = cv2.getTickCount()
    time1 = (t2-t1)/freq
    frame_rate_calc= 1/time1

    # Press 'q' to quit
    if cv2.waitKey(1) == ord('q'):
        break

# Clean up
cv2.destroyAllWindows()
videostream.stop()

Save it as TFLite_detection_webcam.py in the ~/Projects/Python/tflite/object_detection folder. In a terminal window, activate the tflite-env virtual environment (if it’s not already activated) and run the program, setting the modeldir parameter to the location of your .tflite and labelmap files.

Copy Code
cd ~/Projects/Python/tflite
source tflite-env/bin/activate
cd object_detection
python TFLite_detection_webcam.py --modeldir=coco_ssd_mobilenet_v1

After a moment, you should see a new window pop up, giving you a feed of the Pi camera or webcam. If it seems a little blurry, you can use a pair of needle nose pliers to carefully rotate the lens to adjust the focus.

Adjusting Raspberry Pi Camera module focus

Try pointing the camera at various objects to see if the program can recognize them!

SSD object detection on Raspberry Pi

Note that the model is not always the most accurate.

That is a dog

It generally works better if objects look closer to the original images used in the COCO dataset and under similar lighting conditions. If you are training your own model, you can generally control those aspects to make the model more accurate.

Rather than training from scratch, you can also employ transfer learning where certain variables or layers of a pre-trained model are tweaked to recognize objects from your own dataset. This works best if objects are close to the ones in the original training dataset. We will cover transfer learning in a future tutorial.

Resources and Going Further

I hope this has helped you get started with object detection for your own projects! To assist you, here are a few extra resources that might be worth looking at:

 

Référence fabricant SC0023
RPI CAM V2 IMX219 8MP
Raspberry Pi
Référence fabricant SC0073
SBC 1.4GHZ 4 CORE 1GB RAM
Raspberry Pi
Référence fabricant SC0194(9)
SBC 1.5GHZ 4 CORE 4GB PI 4 MOD B
Raspberry Pi
Référence fabricant SC0195(9)
SBC 1.5GHZ 4 CORE 8GB PI 4 MOD B
Raspberry Pi
140,23 €
Afficher plus Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.