Maker.io main logo

How to Make an LED Flower Power Hair Accessory

28

2024-06-20 | By Kitronik Maker

License: See Original Project LEDs / Discrete / Modules

Courtesy of Kitronik

Guide by Kitronik Maker

Description

Add a bit of fun to a flower hair accessory by inserting an LED into the centre. As ‎the flower is quite small there is only space for a small circuit to be hidden on the ‎back. The miniature cell holder is therefore an ideal component for this project as it ‎can be tucked away very discreetly. This circuit has no switch, so the battery has ‎to be removed in order to switch the LED off.‎

project_1

hair_2

Learn how to:‎

• Create a basic circuit using a standard LED and miniature cell holder.‎

Level of difficulty:‎

• Beginner

Parts list

In order to make your LED flower power hair accessory you will need:‎

parts_3

You will also need the following equipment:‎

 

Step by Step guide to making an LED flower power ‎hair accessory

Step 1‎

step1_4

Use a braddle or drill to carefully make a hole in the centre of the flower.‎

step1_5

Flower hair accessories might look delicate, but most have plastic or metal centres ‎holding them together. Try to choose one that doesn’t feel too thick in the centre.‎

Step 2‎

step2_6

Push both legs of the LED through the hole to the back of the flower. Use round ‎nosed pliers to twist the negative leg into a small loop.‎

step2_7

Use conductive thread to oversew stitches to stitch the negative leg to the flower. ‎Make sure the stitches are tight to ensure a good connection.‎

step2_8

Using the same length of thread stitch small running stitches to the position where ‎the cell holder will be. Oversew the negative side of the cell holder to the backing ‎fabric. Note there are two holes on the negative side of the cell holder. Use the one ‎with the silver rim. The other hole is stitched using ordinary thread and is there to ‎add stability rather than being part of the circuit. Finish off the thread neatly at the ‎end making sure there are no loose tails.‎

Step 3‎

step3_9

Use round nosed pliers to twist the positive leg into a loop. Make sure the legs of ‎the LED aren’t touching as this will short out the circuit.‎

step3_10

Using a new piece of thread oversew the positive leg to the flower.‎

step3_11

Using the same thread stitch small running stitches to reach the positive side of ‎the cell holder and oversew it in place. Note there are two holes on the positive ‎side of the cell holder. Use the one with the silver rim. The other hole is stitched ‎using ordinary thread and is there to add stability rather than being part of the ‎circuit. As the flower is small the distance between parts of the circuit is short. ‎Take extra care to make sure the positive and negative sides of the circuit don’t ‎touch.‎

Step 4‎

step4_12

Use ordinary sewing thread to stitch the remaining holes in the cell holder. These ‎just provide stability rather than being part of the circuit.‎

Step 5

step5_13

Slide the cell into the cell holder with the positive side facing upwards. If you don’t ‎want the circuit to be visible on the back of the flower, use a piece of non-fraying ‎fabric to create a cover. Poppers or small strips of hook and loop fastener attached ‎to the fabric would allow access to the battery. Download a pdf version of this ‎page here. This tutorial was produced for Kitronik by Julie Boyd who is a specialist ‎in e-textiles design.‎

‎©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik's prior written consent.

Référence fabricant 2718
SEWABLE MINIATURE COIN CELL HOLD
Kitronik Ltd.
Référence fabricant INL-3AW30
LED WHITE CLEAR 3MM T/H
Inolux
Référence fabricant 2744
ELECTRO-FASHION, CONDUCTIVE THRE
Kitronik Ltd.
Référence fabricant 2443P
2443P ROUND NOSE PLIER 146 MM
Apex Tool Group
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.