Maker.io main logo

Garmin LIDAR-Lite v4 (Qwiic) Hookup Guide

116

2021-06-22 | By SparkFun Electronics

License: See Original Project Programmers

Courtesy of SparkFun

Guide by SANTA CLAUS IMPERSONATOR, MAKIN-STUFF

Introduction

The new Garmin® LIDAR sensor is now easier to use, as a Qwiic device. The Garmin® LIDAR-Lite v4 (Qwiic), fuses the advanced measurement technology of Garmin®'s LIDAR-Lite v4 sensor with the simplicity of SparkFun's Qwiic connect system, for rapid prototyping.

Garmin LIDAR-Lite v4 LED - Distance Measurement Sensor (Qwiic)

The LIDAR sensor is ideal for drone, robot, IoT, or unmanned vehicle operations, with a range up to 10 meters and 1 cm resolution. Check out the video below for an overview of the product features.

 

Required Materials

The Qwiic LIDAR-Lite v4 does need a few additional items for you to get started. The RedBoard Qwiic will be used for the Arduino examples. You may already have a few of these items, including the required Qwiic cable, so feel free to modify your cart based on your needs. Additionally, there are also alternative parts options that are available as well.

ALTERNATIVE PARTS

Qwiic Compatible Microcontrollers:

In addition, we also offer, Qwiic compatible stackable shields for microcontrollers that don't include a Qwiic connector.

You will also need a Qwiic cable to connect to your Qwiic device, choose a length that suits your needs.

Suggested Reading

If you're unfamiliar with serial terminals, jumper pads, or I2C be sure to check out some of these foundational tutorials.

  • Installing an Arduino Library: How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

  • Installing Arduino IDE: A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.

  • Logic Levels: Learn the difference between 3.3V and 5V devices and logic levels.

  • I2C: An introduction to I2C, one of the main embedded communications protocols in use today.

  • Serial Terminal Basics: This tutorial will show you how to communicate with your serial devices using a variety of terminal emulator applications.

  • How to Work with Jumper Pads and PCB Traces: Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.

  • RedBoard Qwiic Hookup Guide: This tutorial covers the basic functionality of the RedBoard Qwiic. This tutorial also covers how to get started blinking an LED and using the Qwiic system.

  • Arduino Shields v2: An update to our classic Arduino Shields Tutorial! All things Arduino shields. What they are and how to assemble them.

Qwiic_1

The Garmin LIDAR-Lite v4 (Qwiic) utilizes the Qwiic connect system. We recommend familiarizing yourself with the Logic Levels and I2C tutorials (above) before using it.

 

 

Hardware Overview

Board Dimensions

The Garmin LIDAR-Lite v4 (Qwiic) has an attached 1" x 1" Qwiic board for ease of use. The overall product dimensions are approximately 2.8" x 1.0" x 0.9" (L x W x H), with more detailed measurements in the drawing below.

Drawing_2

Board dimensions (PDF) for the Garmin LIDAR-Lite v4 (Qwiic), in inches

Mounting Options

The Garmin LIDAR-Lite v4 operation manual lists zip ties and double-sided tape as attachment methods. There are notches on the sensor housing that appear to be meant for a zip tie.

Mount_3

Screw holes and zip-tie notches on the Qwiic LIDAR-Lite v4

With our Qwiic version, we provide two screw holes on the Qwiic board as an additional mounting option. The holes are compatible with 4-40 screws and hardware.

Power

There is a power status LED to indicate when the Garmin LIDAR-Lite v4 (Qwiic) sensor is powered. Power the board either through the polarized Qwiic connector system or the breakout pins (3.3V or 5V and GND) provided. The Qwiic system is meant to run on 3.3V, be sure that you are NOT using another voltage when using the Qwiic system. A jumper is available on the back of the board to remove power to the LED for low-power applications (see Jumpers section below).

Power_4

Power LED and power breakout pins on the Qwiic LIDAR-Lite v4

DC-DC Converter

The Garmin LIDAR-Lite v4 sensor requires 5V to operate. In order to provide 5V to the sensor from the 3.3V line of the Qwiic connector, a DC-to-DC voltage converter is utilized. This can also be referred to as the buck/boost converter/circuit. For more details, check out the XC9140 datasheet.

Converter_5

Boost converter on the Qwiic LIDAR-Lite v4

Garmin LIDAR-Lite v4

The Garmin® LIDAR-Lite v4 is a distance measurement sensor. For more details on the sensor, please refer to the operation manual and technical specifications.

LIDAR_6

Garming® LIDAR-Lite v4 sensor

Note: For the sensor's compliance and safety information, please refer to the safety and product information documentation.

Sensor Characteristics

Note: The power and current consumption characteristics listed below are from the operation manual and technical specifications. However, these specifications are for the sensor itself.

To prevent brown outs, users should be wary when attaching several Qwiic LIDAR-Lite v4s to the Qwiic connect system. Users can easily surpass the current (supply) limitation of their Qwiic microcontroller board. The Qwiic LIDAR-Lite v4 operates at 3.3V and we have measured the current consumption from the 3.3V line to be approximately:

  • 120mA (idle)

  • 165mA (during an acquisition)

Below, are the LIDAR sensor's electrical and performance characteristics, as listed in the operation manual and technical specifications datasheet.

Table_7

*NOTE: As measured indoors to a 90% reflective target; 1 cm is equivalent to 1 standard deviation. Measurements were obtained using high accuracy mode.

Qwiic and I2C

I2C Address

The Garmin LIDAR-Lite v4 (Qwiic)’s I2C address, 0x62 (7-bit), is factory set. However, this address is software configurable.

Qwiic Connectors

The simplest way to use the Garmin LIDAR-Lite v4 (Qwiic) is through the Qwiic connect system. The connectors are polarized for the I2C connection and power. (*They are tied to the corresponding power and I2C breakout pins.)

Connectors_8

Qwiic connectors on the Qwiic LIDAR-Lite v4

Breakout Pins

Note: Excluding the 5V pin, the rest are 3.3V pins.

The board also provides eleven labeled breakout pins. Besides the 5V (and GND) pin, the rest of the pins are only 3.3V tolerant.

I2C

You can connect these lines to the I2C bus of your microcontroller and power pins (3.3V and GND) if it doesn't have a Qwiic connector. The interrupt pins are also broken out to use for triggered events.

I2C_9

I2C Connections- The pins are tied to the Qwiic connectors

J-Link Debug and I/O Pins

DANGER!

Reprogramming the nRF52840 System on Chip (SoC) removes all pre-programmed factory software. SparkFun is NOT able to help you recover the software once it has been removed.

Before attempting to mess with the the nRF52840 System on Chip (SoC), we highly recommend users refer to the operation manual and technical specifications for other considerations and notices from the manufacturer.

The J-Link and I/O pins are also broken out for users in case they wish to interface with the RF52840 SoC.

Pins_10

Other breakout pins on the Qwiic LIDAR-Lite v4

Jumpers

There are three jumpers on the board. Not sure how to cut or modify a jumper? Read here!

  • Power LED - Cutting the LED jumper will remove the 1kΩ resistors and PWR LED from the 3.3V power. This is useful for lowering power consumption.

  • I2C Pull-Up - Cutting the I2C jumper will remove the 4.7kΩ pull-up resistors from the I2C bus. If you have many devices on your I2C bus you may want to remove these jumpers.

  • 5V Disconnect - Cutting the 5V jumper on the board will disconnect the buck converter from the 5V power trace. This is useful when users power the board through the 5V breakout pin.

Jumpers_11

The power LED, I2C pull-up resistor, and 5V disconnect jumpers on the Qwiic LIDAR-Lite v4

Hardware Assembly

With the Qwiic connector system, assembling the hardware is simple. All you need to do is connect your Garmin LIDAR-Lite v4 (Qwiic) to the RedBoard Qwiic with a Qwiic cable. Otherwise, you can use the I2C pins of your microcontroller; just be aware of logic levels.

System_12

RedBoard Qwiic connected the Qwiic LIDAR-Lite v4 with a Qwiic cable

Arduino Library

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

We've written a library to easily get setup and take readings from the Garmin LIDAR-Lite v4 (Qwiic). However, before we jump into retrieving measurements from the sensor, let's take a closer look at the available functions in the library. You can install this library through the Arduino Library Manager. Search for SparkFun Garmin LIDAR-Lite v4 Arduino Library and you should be able to install the latest version. If you prefer manually downloading the libraries from the GitHub repository, you can grab them here:

DOWNLOAD THE SPARKFUN GARMIN LIDAR-LITE V4 ARDUINO LIBRARY

Note: Users may also notice another Arduino for the Garmin LIDAR-Lite. This library is provided and maintained by Garmin®, for all their LIDAR sensors. For more details, check out the GitHub repository.

Library_13

Garmin and SparkFun Arduino libraries for the Garmin LIDAR-Lite v4

Arduino Examples

Example 1: Basic Readings

Once you've got the library installed, open the Example1_GetDistance sketch. You can find it under

Copy Code
File > Examples > SparkFun Garmin LIDAR-Lite v4 Arduino Library > Examples

Then upload the sketch onto your RedBoard or Uno and open your favorite Serial Terminal to see the printed values. (Don't forget to set the baud rate to 115200bps.)

Com_14

Distance readings from the LIDAR sensor

Example 2: Address Change

Note: The Qwiic LIDAR-Lite v4 will reset to the default I2C address if power is disconnected.

Open the Example2_ChangeI2CAddress sketch from the library examples.

Once the sketch has been uploaded, open up a Serial Terminal with the baud rate set at 115200bps. There, users will be prompted to input a value to change the I2C address.

Address_15

Prompt for changing the LIDAR sensor's I2C address

Following the address change, the sketch will scan the I2C bus for connected devices and display their address. Users should see the LIDAR sensor at the address they specified.

Troubleshooting

Below, we have also included some troubleshooting tips for issues that you may come across.

  1. One of our employees compiled a great list of troubleshooting tips based on the most common customer issues. This is the perfect place to start.

  2. For any Arduino IDE specific issues, we recommend starting with their troubleshooting guide.

Not working as expected and need help?

If you need technical assistance and more information on a product that is not working as you expected, we recommend heading on over to the SparkFun Technical Assistance page for some initial troubleshooting.

SPARKFUN TECHNICAL ASSISTANCE PAGE

If you can't find what you need there, you'll need a Forum Account to search product forums and post questions.

Resources and Going Further

Référence fabricant 18009
GARMIN LIDAR-LITE V4 LED - DISTA
SparkFun Electronics
101,95 €
Afficher plus Details
Référence fabricant 15776
SENSOR OPTICAL 40M I2C, SPI
SparkFun Electronics
Référence fabricant 15123
REDBOARD QWIIC ATMEGA328 EVAL BD
SparkFun Electronics
Référence fabricant 15081
QWIIC CABLE KIT
SparkFun Electronics
Référence fabricant U050AB-006-WH
CBL USB2.0 A PLUG-MCR B PLUG 6'
Eaton Tripp Lite
Référence fabricant 15663
SPARKFUN THING PLUS ESP32 WROOM
SparkFun Electronics
Référence fabricant 15795
SPARKFUN QWIIC PRO MICRO - USB-C
SparkFun Electronics
Référence fabricant 15444
REDBOARD ARTEMIS
SparkFun Electronics
Référence fabricant 14713
THING PLUS - SAMD51
SparkFun Electronics
Référence fabricant 14495
QWIIC ADAPTER
SparkFun Electronics
Référence fabricant 16790
QWIIC SHIELD FOR THING PLUS
SparkFun Electronics
Référence fabricant 16789
QWIIC SHIELD FOR ARDUINO NANO
SparkFun Electronics
Référence fabricant 17119
SPARKFUN QWIIC SHIELD FOR TEENSY
SparkFun Electronics
Référence fabricant 14427
QWIIC CABLE - 100MM
SparkFun Electronics
Référence fabricant 14426
QWIIC CABLE - 50MM
SparkFun Electronics
Référence fabricant 14428
QWIIC CABLE - 200MM
SparkFun Electronics
Référence fabricant 14429
QWIIC CABLE - 500MM
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.