Maker.io main logo

Clue Coffee Scale

150

2024-06-28 | By Adafruit Industries

License: See Original Project Programmers STEMMA

Courtesy of Adafruit

Guide by Jan Goolsbey

Overview

cup_1

Consistently brewing that crowning cup of coffee involves attention ‎to the precise addition of ingredients and control of the brew ratio, ‎tempered with practiced technique. Perhaps it's time to apply a little ‎more science to the art.‎

The Clue Coffee Scale can accurately measure the weight of the ‎ground beans or the extraction output, getting closer to an exact and ‎repeatable approach for creating your preferred brew. To measure ‎the contents of a container, the scale can be zeroed with a push of a ‎button to subtract the container's tare weight.‎

The scale uses a load cell sensor device that consists of a very ‎sensitive resistance array (a strain gauge) attached to a metal ‎bending beam. When connected to an exciter voltage, the resistance ‎array provides a differential voltage output signal proportional to the ‎torque of the mass placed on the load cell. The signal voltage is very ‎low so a sensitive amplifier and high-resolution analog to digital ‎converter (ADC) are used to provide a microcontroller-compatible ‎measurement.‎

The Adafruit NAU7802 24-Bit ADC - STEMMA QT board has ‎everything needed to connect a load cell and provide measurements ‎for the Clue. Add a CircuitPython program, and the Clue Coffee Scale ‎is born.‎

John Park built a version of the coffee scale for use with his primo ‎espresso station. Check out the Build the Coffee Scale section of this ‎guide for the step-by-step approach he used for his custom scale. ‎A trenta-sized thank you goes to John for creating a practical and ‎beautiful working scale.‎

This guide will show how to build, calibrate, and code the scale. Your ‎perfect cup of Java awaits.‎

force___flex_espresso_action

A load cell is a precision device particularly when it is paired with a ‎sensitive high-resolution ADC such as the NAU7802. However, ‎because of component variations and software accuracy limitations, ‎the scale SHOULD NOT BE USED for safety, health, scientific, or ‎commercial weight measurement applications.‎

Parts

Features and Operation

features_2

The User Interface

  • The Clue Coffee Scale continuously displays the load cell weight ‎measurement in both grams and ounces.‎
  • The five-division graduated scale in the center of the display is ‎calibrated in grams and shows the measured weight relative to ‎the maximum value of 100 grams (default).‎
  • The indicator bubble travels up and down the graduated scale, ‎pointing to the currently measured value in grams. The interior ‎of the indicator bubble will turn red if the measured value is ‎outside of the graduated scale range.‎
  • The Clue A button is used to zero or tare the scale. Press the ‎button until a beep is heard, then release. The interior of the ‎bubble and the Clue's NeoPixel will turn red while ‎zeroing/taring. A second beep is heard when the scale ‎completes the zero/tare process.‎

Build the Coffee Scale

build_3

This is one specific implementation of the scale for use on an ‎espresso machine. Your build will vary depending on the target ‎machine.‎

machine_4

Attach Plates

In an attempt to make a minimal scale to integrate with the ‎espresso machine's drip tray, only two pieces of aluminum, the load ‎cell, and a few fasteners are used.‎

The fixed end of the load cell (the side with the wires) is tapped with ‎M5 screw holes, while the weighing end that can flex is tapped with ‎M4.‎

Using an M4 screw, attach the large cross-plate to the underside of ‎the load cell. (Note the sticker on the end of the cell with the load ‎rating and arrow.)‎

Then, attach the 3-hole coupling plate with an M5 screw to the ‎underside of the load cell at the fixed end.‎

plate_5

plate_6

plate_7

plate_8

screw_9

Mount Scale to Drip Tray Grid

Use M3 screws, spacers, and nuts to attach the coupling plate to the ‎drip tray grid as shown.‎

The spacers are necessary to give the load cell clearance to flex ‎under load as shown in the fourth picture here.‎

mount_10

mount_11

mount_12

mount_13

mount_14

Wire Prep

If you like, you can add some short lengths of heat shrink tubing to ‎collect the four wires, as well as add small ferrules to their ends -- ‎this makes it easier to connect them to the screw terminals on the ‎ADC board.

prep_15

These wires are so thin you may want to solder them to the inside of ‎the ferrules at the tip rather than crimp them.‎

solder_16

Clue Connection

Add the Clue case to the clue but leave off one screw in the upper ‎right corner.‎

Use a longer M2.5 screw and nut to connect the ADC board to the ‎back of the Clue.‎

Then, connect the Clue and ADC via STEMMA QT cable.‎

clue_17

clue_18

clue_19

clue_20

Clue Mount

Mount the 2020 corner brace to the front of the drip tray grid using ‎an M3 screw, nut, and washer or spacer.‎

Then mount the Clue to the brace using the remaining M3 nylon ‎screw and nut from the acrylic case kit.‎

brace_21

brace_22

brace_23

brace_24

brace_25

Battery Pack

Connect the AAA battery pack to the Clue. Then, use the adhesive ‎square to connect the battery pack lid to the drip tray's side.‎

This will allow you to pull out the battery pack to change the ‎batteries when needed.‎

battery_26

battery_27

battery_28

battery_29

CircuitPython on CLUE

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY flash drive to iterate.‎

The following instructions will show you how to install CircuitPython. ‎If you've already installed CircuitPython but are looking to update it ‎or reinstall it, the same steps work for that as well!‎

Set up CircuitPython Quick Start!‎

Follow this quick step-by-step for super-fast Python power :)‎

Download the latest version of CircuitPython for CLUE from ‎circuitpython.org

Click the link above to download the latest version of ‎CircuitPython for the CLUE.‎

Download and save it to your desktop (or wherever is handy).‎

download_30

Plug your CLUE into your computer using a known-good USB cable.‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! So make sure you have a USB cable you know is good ‎for data sync.‎

Double-click the Reset button on the top (magenta arrow) on your ‎board, and you will see the NeoPixel RGB LED (green arrow) turn ‎green. If it turns red, check the USB cable, try another USB port, ‎etc. Note: The little red LED next to the USB connector will pulse red. ‎That's ok!‎

If double-clicking doesn't work the first time, try again. Sometimes it ‎can take a few tries to get the rhythm right!‎

board_31

You will see a new disk drive appear called CLUEBOOT.‎

Drag the adafruit-circuitpython-clue-etc.uf2 file to CLUEBOOT.‎

drive_32

drive_33

The LED will flash. Then, the CLUEBOOT drive will disappear, and a ‎new disk drive called CIRCUITPY will appear.‎

If this is the first time, you're installing CircuitPython or you're doing ‎a completely fresh install after erasing the filesystem, you will have ‎two files - boot_out.txt, and code.py, and one folder - lib on ‎your CIRCUITPY drive.‎

If CircuitPython was already installed, the files present before ‎reloading CircuitPython should still be present on ‎your CIRCUITPY drive. Loading CircuitPython will not create new ‎files if there was already a CircuitPython filesystem present.‎

That's it, you're done! :)‎

disk_34

Code the Coffee Scale

First make sure you are running the latest version of Adafruit ‎CircuitPython for your board.‎

Text Editor

Adafruit recommends using the Mu editor for using your ‎CircuitPython code with the Feather. You can get more info in this ‎guide.‎

Alternatively, you can use any text editor that saves text files.‎

Download the Project Bundle

Your Clue Coffee Scale project will use a specific set of CircuitPython ‎libraries, a bitmap image, fonts, a calibration method, and ‎the code.py file. To get everything you need, click on the Download ‎Project Bundle link below, and uncompress the .zip file.‎

bundle_35

Connect your CLUE to your computer via a known good data+power ‎cable. Look for the CIRCUITPY drive which pops up in your Finder or ‎File Explorer (depending on your operating system).‎

Drag the contents of the uncompressed bundle directory onto your ‎Clue board's CIRCUITPY drive, replacing any existing files or ‎directories with the same names, and adding any new ones that are ‎necessary.‎

The Project Bundle contains the following folders and files:‎

  • clue_scale_bkg.bmp the background bitmap image
  • clue_scale_calibrator.py the load cell calibration program ‎code
  • code.py the main Coffee Scale program code
  • fonts folder:
    • Helvetica-Bold-24.bdf font file
    • OpenSans-16.bdf font file
    • OpenSans-9.bdf font file
  • lib folder containing these required libraries:
    • adafruit_apds9960
    • adafruit_bitmap_font
    • adafruit_bmp280
    • adafruit_clue
    • adafruit_display_shapes
    • adafruit_display_text
    • adafruit_lis3mdl
    • adafruit_lsm6ds
    • adafruit_register
    • adafruit_sht31d
    • cedargrove_nau7802‎
    • neopixel
    • simpleio

The cedargrove_nau7802 library driver can also be found in ‎the CircuitPython Community Bundle. For the curious, NAU7802 ‎driver API information is available in Cedar Grove's GitHub repository.‎

code.py

The main CircuitPython code for the Coffee Scale is contained in the ‎project zip folder as code.py. Copy this and all the other bundle files ‎to the main (root) folder of the CIRCUITPY drive that appears when ‎your Clue is connected to your computer via a known good USB ‎cable.‎

Before using the scale, you'll need to update code.py with a ‎calibration ratio that is unique to the load cell attached to the ‎NAU7802 Stemma breakout. See the guide section, Calibrate the ‎Load Cell for instructions. You should only have to measure and ‎record the load cell calibration ratio once.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2023 Jan Goolsbey for Adafruit Industries
# SPDX-License-Identifier: MIT
#
# clue_scale_code.py
# 2023-01-13 v1.2.1
#
# Clue Scale - Single Channel Version
# Adafruit NAU7802 Stemma breakout example

# import clue_scale_calibrator # Uncomment to run calibrator method

import time
import board
from simpleio import map_range
from adafruit_clue import clue
from adafruit_display_shapes.circle import Circle
from adafruit_display_text.label import Label
from adafruit_bitmap_font import bitmap_font
import displayio
from cedargrove_nau7802 import NAU7802

clue.pixel.brightness = 0.2 # Set NeoPixel brightness
clue.pixel[0] = clue.YELLOW # Set status indicator to yellow (initializing)

# Set Scale Defaults
MAX_GR = 100 # Maximum (full-scale) display range in grams
DEFAULT_GAIN = 128 # Default gain for internal PGA
SAMPLE_AVG = 5 # Number of sample values to average
SCALE_NAME_1 = "COFFEE" # 6 characters maximum
SCALE_NAME_2 = "SCALE" # 6 characters maximum

"""Enter the calibration ratio for the individual load cell in-use. The ratio is
composed of the reference weight in grams divided by the raw reading. For
example, a raw reading of 215300 for a 100 gram weight results in a calibration
ratio of 100 / 215300. Use the clue_scale_single_calibrate method to obtain the
raw value.
FYI: A US dime coin weighs 2.268 grams or 0.079 ounces."""
CALIB_RATIO = 100 / 215300 # load cell serial#4540-02

# Instantiate the Sensor and Display
i2c = board.I2C() # uses board.SCL and board.SDA
# i2c = board.STEMMA_I2C() # For using the built-in STEMMA QT connector on a microcontroller
nau7802 = NAU7802(i2c, address=0x2A, active_channels=1)

display = board.DISPLAY
scale_group = displayio.Group()

FONT_0 = bitmap_font.load_font("/fonts/Helvetica-Bold-24.bdf")
FONT_1 = bitmap_font.load_font("/fonts/OpenSans-16.bdf")
FONT_2 = bitmap_font.load_font("/fonts/OpenSans-9.bdf")

# Display the Background Bitmap Image
bkg = displayio.OnDiskBitmap("/clue_scale_bkg.bmp")
_background = displayio.TileGrid(bkg, pixel_shader=bkg.pixel_shader, x=0, y=0)
scale_group.append(_background)

# Define and Display the Text Labels and Graphic Elements
# Place the project name on either side of the graduated scale
scale_name_1 = Label(FONT_1, text=SCALE_NAME_1, color=clue.CYAN)
scale_name_1.anchor_point = (0.5, 0.5)
scale_name_1.anchored_position = (40, 96)
scale_group.append(scale_name_1)

scale_name_2 = Label(FONT_1, text=SCALE_NAME_2, color=clue.CYAN)
scale_name_2.anchor_point = (0.5, 0.5)
scale_name_2.anchored_position = (199, 96)
scale_group.append(scale_name_2)

# Define the zeroing button graphic
zero_button_circle = Circle(14, 152, 14, fill=None, outline=clue.RED, stroke=2)
scale_group.append(zero_button_circle)

zero_button_label = Label(FONT_1, text="Z", color=clue.RED)
zero_button_label.x = 8
zero_button_label.y = 150
scale_group.append(zero_button_label)

# Place tickmark labels next to the graduated scale
for i in range(-1, 6):
tick_value = Label(FONT_2, text=str((MAX_GR) // 5 * i), color=clue.CYAN)
if i == -1:
tick_value.anchor_point = (1.0, 1.1)
elif i == 5:
tick_value.anchor_point = (1.0, 0.0)
else:
tick_value.anchor_point = (1.0, 0.5)
tick_value.anchored_position = (99, 201 - (i * 40))
scale_group.append(tick_value)

# Place the grams and ounces labels and values near the bottom of the display
grams_label = Label(FONT_0, text="grams", color=clue.BLUE)
grams_label.anchor_point = (1.0, 0)
grams_label.anchored_position = (80, 216)
scale_group.append(grams_label)

ounces_label = Label(FONT_0, text="ounces", color=clue.BLUE)
ounces_label.anchor_point = (1.0, 0)
ounces_label.anchored_position = (230, 216)
scale_group.append(ounces_label)

grams_value = Label(FONT_0, text="0.0", color=clue.WHITE)
grams_value.anchor_point = (1.0, 0.5)
grams_value.anchored_position = (80, 200)
scale_group.append(grams_value)

ounces_value = Label(FONT_0, text="0.00", color=clue.WHITE)
ounces_value.anchor_point = (1.0, 0.5)
ounces_value.anchored_position = (230, 200)
scale_group.append(ounces_value)

# Define the moveable indicator bubble
indicator_group = displayio.Group()
bubble = Circle(120, 200, 10, fill=clue.YELLOW, outline=clue.YELLOW, stroke=3)
indicator_group.append(bubble)

scale_group.append(indicator_group)
display.root_group = scale_group


# Helpers
def zero_channel():
"""Prepare internal amplifier settings and zero the current channel. Use
after power-up, a new channel is selected, or to adjust for measurement
drift. Can be used to zero the scale with a tare weight.
The nau7802.calibrate function used here does not calibrate the load cell,
but sets the NAU7802 internals to prepare for measuring input signals."""
nau7802.calibrate("INTERNAL")
nau7802.calibrate("OFFSET")


def read(samples=1):
"""Read and average consecutive raw samples; return averaged value."""
sample_sum = 0
sample_count = samples
while sample_count > 0:
if nau7802.available():
sample_sum = sample_sum + nau7802.read()
sample_count -= 1
return int(sample_sum / samples)


# Activate the Sensor
# Enable the internal analog circuitry, set gain, and zero
nau7802.enable(True)
nau7802.gain = DEFAULT_GAIN
zero_channel()

# Play "welcome" tones
clue.play_tone(1660, 0.15)
clue.play_tone(1440, 0.15)

# The Primary Code Loop
# Read sensor, move bubble, and display values
while True:
clue.pixel[0] = clue.GREEN # Set status indicator to green (ready)

# Read the raw scale value and scale for grams and ounces
value = read(SAMPLE_AVG)
mass_grams = round(value * CALIB_RATIO, 1)
mass_ounces = round(mass_grams * 0.03527, 2)
grams_value.text = f"{mass_grams:5.1f}"
ounces_value.text = f"{mass_ounces:5.2f}"
print(f" {mass_grams:5.1f} grams {mass_ounces:5.2f} ounces")

# Reposition the indicator bubble based on grams value
min_gr = (MAX_GR // 5) * -1 # Minimum display value
bubble.y = int(map_range(mass_grams, min_gr, MAX_GR, 240, 0)) - 10
if mass_grams > MAX_GR or mass_grams < min_gr:
bubble.fill = clue.RED
else:
bubble.fill = None

# Check to see if the zeroing button is pressed
if clue.button_a:
# Zero the sensor
clue.pixel[0] = clue.RED # Set status indicator to red (stopped)
bubble.fill = clue.RED # Set bubble center to red (stopped)
clue.play_tone(1660, 0.3) # Play "button pressed" tone

zero_channel()

while clue.button_a:
# Wait until the button is released
time.sleep(0.1)

clue.play_tone(1440, 0.5) # Play "reset completed" tone
bubble.fill = None # Set bubble center to transparent (ready)

View on GitHub

Code Details

details_36

Clue Coffee Scale Display Design Concept

Let's take a walk through the code and look in more detail how each ‎section works within code.py.‎

The main module, code.py, prepares and operates the Coffee Scale. ‎It consists of the following major sections:‎

  • Import and Set Defaults
  • Calibration Ratio
  • Instantiate the Sensor and Display
  • Display the Background Bitmap Image
  • Define and Display the Text Labels and Graphic Elements
  • Helpers
  • Activate the Sensor and Prepare to Loop
  • The Primary Code Loop

Import and Set Defaults

This section imports all the needed modules and libraries, including ‎the NAU7802 sensor driver. After importing, the first visible task of ‎this section is to turn the Clue NeoPixel to the color yellow to ‎indicate that the Coffee Scale is initializing. During operation, the ‎indicator LED will glow green when operating normally or red when ‎zeroing the scale.‎

Next, the scale defaults are specified. These are constants with ‎names that are capitalized to help identify them as constants. These ‎are values that you can change to alter the operation of the scale.‎

MAX_GR is the full-scale value of the scale in grams. The tick mark ‎values adjacent to the graduated scale graphic are automatically ‎derived from MAX_GR which can by any positive integer value. Since the ‎graduated scale graphic is divided into tenths of full-scale with five ‎tick marks, it's best to choose an integer MAX_GR value that will display ‎nicely such as 1000, 500, 250, 100, 50, 25, 10, or 5.‎

DEFAULT_GAIN is the gain setting of the NAU7802's internal ADC pre-‎amplifier. Normally, this is set to the highest value of 128.‎

SAMPLE_AVG specifies the number of measurements that are averaged ‎when the load cell is measured. The measurement value will be ‎more stable with a high SAMPLE_AVG value. The display will update more ‎slowly with a high value; it's a trade-off between stability and speed.‎

SCALE_NAME_1 is the text string that appears on the display to the left of ‎the graduated scale. This should be no longer than 6 characters. ‎Upper case letters will look the best.‎

SCALE_NAME_2 is the text string that appears on the display to the right of ‎the graduated scale. This should be no longer than 6 characters. ‎Upper case letters will look the best on the display.‎

Download File

Copy Code
# import clue_scale_calibrator  # Uncomment to run calibrator method

import time
import board
from simpleio import map_range
from adafruit_clue import clue
from adafruit_display_shapes.circle import Circle
from adafruit_display_text.label import Label
from adafruit_bitmap_font import bitmap_font
import displayio
from cedargrove_nau7802 import NAU7802

clue.pixel.brightness = 0.2 # Set NeoPixel brightness
clue.pixel[0] = clue.YELLOW # Set status indicator to yellow (initializing)

# Set Scale Defaults
MAX_GR = 100 # Maximum (full-scale) display range in grams
DEFAULT_GAIN = 128 # Default gain for internal PGA
SAMPLE_AVG = 5 # Number of sample values to average
SCALE_NAME_1 = "COFFEE" # 6 characters maximum
SCALE_NAME_2 = "SCALE" # 6 characters maximum

Calibration Ratio

CALIB_RATIO is the factor that is used to convert the NAU7802's raw ‎measurement value into grams. This ratio is updated after running ‎the calibrator method. See the guide section, Calibrate the Load ‎Cell for instructions. You should only have to measure and record the ‎load cell calibration ratio once.‎

Download File

Copy Code
"""Enter the calibration ratio for the individual load cell in-use. The ratio is
composed of the reference weight in grams divided by the raw reading. For
example, a raw reading of 215300 for a 100 gram weight results in a calibration
ratio of 100 / 215300. Use the clue_scale_single_calibrate method to obtain the
raw value.
FYI: A US dime coin weighs 2.268 grams or 0.079 ounces."""
CALIB_RATIO = 100 / 215300 # load cell serial#4540-02

Instantiate the Sensor and Display

The NAU7802 Stemma board is connected to the Clue's I2C bus and ‎lives at address 42 (hexadecimal 2A). The NAU7802 24-bit ADC ‎‎(analog to digital converter) chip is a dual-channel device, but only ‎the first channel is available on the Stemma board; active_channels is set ‎to 1.‎

Next, the Clue's integrated display is instantiated along with the ‎primary displayio graphics group layer, scale_group which will contain ‎the background bitmap image and other group layers.‎

The three font objects for display titles, labels, and measurements ‎are listed as constants that will be used when display labels are ‎defined.‎

Download File

Copy Code
# Instantiate the Sensor and Display
nau7802 = NAU7802(board.I2C(), address=0x2A, active_channels=1)

display = board.DISPLAY
scale_group = displayio.Group()

FONT_0 = bitmap_font.load_font("/fonts/Helvetica-Bold-24.bdf")
FONT_1 = bitmap_font.load_font("/fonts/OpenSans-16.bdf")
FONT_2 = bitmap_font.load_font("/fonts/OpenSans-9.bdf")

Display the Background Bitmap Image

The display background containing the graduated scale is loaded ‎from the Clue root directory and is appended as the first item in the ‎primary displayio group layer. All other graphics objects such as ‎labels and the indicator bubble will be put on layers above the ‎background.‎

display_37

Download File

Copy Code
# Display the Background Bitmap Image
bkg = displayio.OnDiskBitmap("/clue_scale_bkg.bmp")
_background = displayio.TileGrid(bkg, pixel_shader=bkg.pixel_shader, x=0, y=0)
scale_group.append(_background)

Define and Display the Text Labels and ‎Graphic Elements

force___flex_raw_display_images_animation

Text Label and Graphic Element Layers in Action

This code section defines the graphic elements that will be placed ‎on the display in front of the background graphic. First, the scale ‎name text and zeroing button graphics are appended to the ‎primary displayio group.‎

The subsection that starts with for i in range... is the code that steps ‎through the graduated scale's tick marks, creating a value label ‎calculated using the MAX_GR constant and appending them to ‎the displayio group. Measurement values and units labels added ‎next.‎

Lastly, the displayio indicator_group and it's floating indicator bubble is ‎created and added to the primary displayio group. ‎The indicator_group becomes the front-most graphics layer of the ‎display.‎

The indicator bubble is a yellow circle that travels up and down the ‎graduated scale, pointing to the measured value. The center of the ‎circle will normally be transparent but will appear yellow or red ‎depending on the scale's current status; yellow when initializing, red ‎when zeroing.‎

Download File

Copy Code
# Define and Display the Text Labels and Graphic Elements
# Place the project name on either side of the graduated scale
scale_name_1 = Label(FONT_1, text=SCALE_NAME_1, color=clue.CYAN)
scale_name_1.anchor_point = (0.5, 0.5)
scale_name_1.anchored_position = (40, 96)
scale_group.append(scale_name_1)

scale_name_2 = Label(FONT_1, text=SCALE_NAME_2, color=clue.CYAN)
scale_name_2.anchor_point = (0.5, 0.5)
scale_name_2.anchored_position = (199, 96)
scale_group.append(scale_name_2)

# Define the zeroing button graphic
zero_button_circle = Circle(14, 152, 14, fill=None, outline=clue.RED, stroke=2)
scale_group.append(zero_button_circle)

zero_button_label = Label(FONT_1, text="Z", color=clue.RED)
zero_button_label.x = 8
zero_button_label.y = 150
scale_group.append(zero_button_label)

# Place tickmark labels next to the graduated scale
for i in range(-1, 6):
tick_value = Label(FONT_2, text=str((MAX_GR) // 5 * i), color=clue.CYAN)
if i == -1:
tick_value.anchor_point = (1.0, 1.1)
elif i == 5:
tick_value.anchor_point = (1.0, 0.0)
else:
tick_value.anchor_point = (1.0, 0.5)
tick_value.anchored_position = (99, 201 - (i * 40))
scale_group.append(tick_value)

# Place the grams and ounces labels and values near the bottom of the display
grams_label = Label(FONT_0, text="grams", color=clue.BLUE)
grams_label.anchor_point = (1.0, 0)
grams_label.anchored_position = (80, 216)
scale_group.append(grams_label)

ounces_label = Label(FONT_0, text="ounces", color=clue.BLUE)
ounces_label.anchor_point = (1.0, 0)
ounces_label.anchored_position = (230, 216)
scale_group.append(ounces_label)

grams_value = Label(FONT_0, text="0.0", color=clue.WHITE)
grams_value.anchor_point = (1.0, 0.5)
grams_value.anchored_position = (80, 200)
scale_group.append(grams_value)

ounces_value = Label(FONT_0, text="0.00", color=clue.WHITE)
ounces_value.anchor_point = (1.0, 0.5)
ounces_value.anchored_position = (230, 200)
scale_group.append(ounces_value)

# Define the moveable indicator bubble
indicator_group = displayio.Group()
bubble = Circle(120, 200, 10, fill=clue.YELLOW, outline=clue.YELLOW, stroke=3)
indicator_group.append(bubble)

scale_group.append(indicator_group)
display.root_group = scale_group

Helpers

These two helper functions work with the NAU7802 driver class to ‎zero the scale and to read the load cell's current raw value.‎

The zero_channel( ) helper sets up and zeros the NAU7802's internal ‎amplifiers and ADC (analog to digital converter) to prepare it to ‎receive signals. This function is used when the scale is first powered-‎up as well as when manually zeroed by pressing the Clue's button A. ‎

The load cell's raw measurement value is obtained by ‎the read( ) helper. This helper accepts an integer parameter that ‎specifies the number of samples to be averaged each time the ‎helper is called, defaulting to 1 sample (no averaging). The helper ‎returns the averaged raw measurement value. Since the NAU7802's ‎internal ADC has 24-bit accuracy, the raw value can range from ‎about -8.3M to + 8.3M.‎

Download File

Copy Code
# Helpers
def zero_channel():
"""Prepare internal amplifier settings and zero the current channel. Use
after power-up, a new channel is selected, or to adjust for measurement
drift. Can be used to zero the scale with a tare weight.
The nau7802.calibrate function used here does not calibrate the load cell,
but sets the NAU7802 internals to prepare for measuring input signals."""
nau7802.calibrate("INTERNAL")
nau7802.calibrate("OFFSET")


def read(samples=1):
"""Read and average consecutive raw samples; return averaged value."""
sample_sum = 0
sample_count = samples
while sample_count > 0:
if nau7802.available():
sample_sum = sample_sum + nau7802.read()
sample_count -= 1
return int(sample_sum / samples)

Activate the Sensor and Prepare to Loop

This is where the NAU7802 ADC is enabled and calibrated for use. ‎Before calibrating and zeroing, the internal sensor amplifier's gain is ‎set to the default value. Once completed, the Clue will chirp some ‎welcoming notes.‎

Download File

Copy Code
# Activate the Sensor
# Enable the internal analog circuitry, set gain, and calibrate/zero
nau7802.enable(True)
nau7802.gain = DEFAULT_GAIN
zero_channel()

# Play "welcome" tones
clue.play_tone(1660, 0.15)
clue.play_tone(1440, 0.15)

The Primary Code Loop

The primary loop is the operational process of the scale. The loop ‎indicates the scale's status on the Clue NeoPixel; green when the ‎scale is operating, red when it's busy zeroing.‎

After setting the NeoPixel to green, the load cell raw value is ‎measured and converted to grams and ounces. The converted ‎values are formatted and placed into the corresponding display ‎labels and is printed in the REPL.‎

The grams measurement value is used to position the on-screen ‎indicator bubble along the graduated scale graphic using ‎the map_range( ) function. Also, if the grams measurement value falls ‎outside of the minimum or maximum range, the bubble is "parked" ‎at the extreme position and its interior color is changed from ‎transparent to red.‎

Finally, the Clue A button is watched to see if it has been pressed. ‎When pressed, the Clue will play a sound and will begin zeroing the ‎scale. During the zeroing process, the NeoPixel and the center of the ‎bubble are set to a red color. When zeroing is completed, the code ‎will wait until the button is released before playing a completion ‎sound, setting the bubble interior to transparent, and returning to ‎normal operation.‎

‎Download File‎

Copy Code
# The Primary Code Loop
# Read sensor, move bubble, and display values
while True:
clue.pixel[0] = clue.GREEN # Set status indicator to green (ready)

# Read the raw scale value and scale for grams and ounces
value = read(SAMPLE_AVG)
mass_grams = round(value * CALIB_RATIO, 1)
mass_ounces = round(mass_grams * 0.03527, 2)
grams_value.text = f"{mass_grams:5.1f}"
ounces_value.text = f"{mass_ounces:5.2f}"
print(f" {mass_grams:5.1f} grams {mass_ounces:5.2f} ounces")

# Reposition the indicator bubble based on grams value
min_gr = (MAX_GR // 5) * -1 # Minimum display value
bubble.y = int(map_range(mass_grams, min_gr, MAX_GR, 240, 0)) - 10
if mass_grams > MAX_GR or mass_grams < min_gr:
bubble.fill = clue.RED
else:
bubble.fill = None

# Check to see if the zeroing button is pressed
if clue.button_a:
# Zero the sensor
clue.pixel[0] = clue.RED # Set status indicator to red (stopped)
bubble.fill = clue.RED # Set bubble center to red (stopped)
clue.play_tone(1660, 0.3) # Play "button pressed" tone

zero_channel()

while clue.button_a:
# Wait until the button is released
time.sleep(0.1)

clue.play_tone(1440, 0.5) # Play "reset completed" tone
bubble.fill = None # Set bubble center to transparent (ready)

Calibrate the Load Cell

calibrate_38

Calibrating the Load Cell with a 100 gram Reference Weight

Calibrator

Before putting the scale to use at your coffee-making station, use a ‎known weight to record the unique resistance characteristics of the ‎load cell sensor. This calibration should only need to be performed ‎once.‎

The calibration process reads and averages a handful of raw ‎measurement samples then prints the averaged value in the serial ‎output window. The printed raw measurement value that ‎corresponds to a reference weight will be used within the scale's ‎CircuitPython code to calculate the grams and ounces displayed on ‎the scale's screen.‎

Remember to mount the load cell so that the fixed end is securely ‎fastened, and the weighing end is free to flex with no restrictions.‎

1. To begin the calibration process, remove all weights from the load ‎cell.

2. The next step is to edit code.py to activate the calibrator method. ‎Using Mu or your favorite text editor (Atom is shown in the example), ‎open the code.py file stored in the root directory of the Clue board ‎and also open a serial output window.‎

process_39

3. Remove the left-most comment hashmark and the following ‎space character from line 10 of the file.‎

process_40

‎4. After making the change to line 10, save the file. The calibration ‎method will automatically run when the code.py file is saved.‎

A notice that the calibrator is ready will print to the serial output ‎window.‎

notice_41

5. Place a reference weight on the measurement end of the load cell. ‎Once a few RAW VALUE measurements are taken, choose one that ‎looks typically like a median value. In this example, the 100-gram ‎reference weight is producing a raw measurement value of ‎approximately 215300.‎

If you need to re-zero the load cell to get a fresh measurement, ‎remove any weights then press and hold the Clue A button until you ‎hear a confirming beep. Release the button and the calibrator will ‎start the internal zeroing process. You'll hear a confirming tone when ‎zeroing is complete.‎

After zeroing the NAU780, the raw value measurement will likely ‎hover within +/- 50 counts of zero. That's expected and within the ‎accuracy expectations for the device.‎

value_42

‎6. It's time to edit the code.py file in your editor once again to ‎update the CALIB_RATIO constant on line 38. The ratio is the reference ‎weight in grams divided by the raw value you noted during ‎calibration. In this example, it's 100 / 215300.‎

Don't save the code.py file just yet. There's one more step to go.‎

step_43

‎7. Place a comment hashmark and a space at the beginning of line ‎‎10 to "comment out" the line so that the calibrator method won't be ‎imported the next time code.py executes.‎‎

8. Save the file and close the editor. The code.py program will ‎automatically begin. The Clue Coffee Scale is now ready to go!‎

Calibrator Code Listing

Here's the code listing for the calibrator method. The calibrator is ‎also a good example of a fundamental approach to initiate and read ‎the raw values of a load cell connected to the NAU7802 ADC ‎STEMMA QT board.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2022 Jan Goolsbey for Adafruit Industries
# SPDX-License-Identifier: MIT
#
# clue_scale_calibrator.py
# 2023-01-13 v1.1.1
#
# Clue Scale Calibrator - Single Channel Version
# Adafruit NAU7802 Stemma breakout example

import time
import board
from adafruit_clue import clue
from cedargrove_nau7802 import NAU7802

clue.pixel.brightness = 0.2 # Set NeoPixel brightness
clue.pixel[0] = clue.YELLOW # Set status indicator to yellow (initializing)

SAMPLE_AVG = 3 # Number of sample values to average
DEFAULT_GAIN = 128 # Default gain for internal PGA

# Instantiate 24-bit load sensor ADC
i2c = board.I2C() # uses board.SCL and board.SDA
# i2c = board.STEMMA_I2C() # For using the built-in STEMMA QT connector on a microcontroller
nau7802 = NAU7802(i2c, address=0x2A, active_channels=1)


def zero_channel():
"""Initiate internal calibration and zero the current channel. Use after
power-up, a new channel is selected, or to adjust for measurement drift.
Can be used to zero the scale with a tare weight."""
nau7802.calibrate("INTERNAL")
nau7802.calibrate("OFFSET")


def read(samples=100):
# Read and average consecutive raw sample values; return average raw value
sample_sum = 0
sample_count = samples
while sample_count > 0:
if nau7802.available():
sample_sum = sample_sum + nau7802.read()
sample_count -= 1
return int(sample_sum / samples)


# Activate the NAU780 internal analog circuitry, set gain, and calibrate/zero
nau7802.enable(True)
nau7802.gain = DEFAULT_GAIN # Use default gain
zero_channel() # Calibrate and zero

print("-----------------------------------")
print(" NAU7802 SINGLE CHANNEL CALIBRATOR")
print("-----------------------------------")
print("Place a calibration weight on the")
print("load cell.")
print("To re-zero the load cell, remove")
print("any weights then press and hold A.")
print("-----------------------------------")
print("")

# Play "welcome" tones
clue.play_tone(1660, 0.15)
clue.play_tone(1440, 0.15)

# Main loop: Read sample and display value
while True:
clue.pixel[0] = clue.GREEN # Set status indicator to green

# Read the raw value; print raw value, gain setting, and % of full-scale
value = read(SAMPLE_AVG)
print(f"CHAN_{nau7802.channel:1.0f} RAW VALUE: {value:7.0f}")
print(f"GAIN: x{DEFAULT_GAIN} full-scale: {(value / ((2**23) - 1)) * 100:3.2f}%")
print("===================================")

time.sleep(0.1)

if clue.button_a:
# Zero and recalibrate the NAU780
clue.play_tone(1660, 0.3) # Play "button pressed" tone
clue.pixel[0] = clue.RED # Set status indicator to red (stopped)
zero_channel()
while clue.button_a:
# Wait until button is released
time.sleep(0.1)
print("RECALIBRATED")
clue.play_tone(1440, 0.5) # Play "reset completed" tone

View on GitHub

Référence fabricant 4538
ADAFRUIT NAU7802 24-BIT ADC - ST
Adafruit Industries LLC
Référence fabricant 4500
CLUE NRF52840 EXPRESS
Adafruit Industries LLC
Référence fabricant 4540
SENSOR FORCE 1KGF DIAPHRAGM
Adafruit Industries LLC
Référence fabricant 4210
JST SH 4-PIN CABLE - QWIIC COMPA
Adafruit Industries LLC
Référence fabricant 727
BATTERY HOLDER AAA 3 CELL LEADS
Adafruit Industries LLC
Référence fabricant 592
CABLE A PLUG TO MCR B PLUG 3'
Adafruit Industries LLC
Référence fabricant 5131
WIRE FERRULE KIT - 800 PIECES
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.