Maker.io main logo

Build Your Own Raspberry Pi Flight Tracker

556

2023-03-16 | By Nate_Larson

License: See Original Project Raspberry Pi SBC

Have you ever looked at a plane flying overhead and wondered where it was going? Where it came ‎from? Did you know you can easily find out and help track aircraft using a Raspberry Pi?‎

All you need to put together a Raspberry Pi flight tracker is a Raspberry Pi, power supply, microSD card, ‎and a Software Defined Radio (SDR) with Automatic Dependent Surveillance-Broadcast (ADS-B) ‎support, such as the RTL2832-based SDR I received some time back in AdaBox007.‎

ADS-B information is transmitted by aircraft to provide identification and altitude information to other ‎aircraft as well as ground-based air traffic control stations. Using an SDR, we can receive this data, and ‎when paired with the data from other receivers using a service such as FlightRadar24, the position of ‎the aircraft can be triangulated.‎

Raspberry Pi Flight Tracker

Setup the Operating System

To create your own flight tracker, begin by flashing your microSD card with the latest version of ‎Raspberry Pi OS using the Raspberry Pi Imager.‎

flashing_1

Before flashing the SD card, open the advanced options by clicking the gear icon.‎

advanced_2

From the advanced options window, set your device’s hostname and password, enable SSH, configure ‎your wireless LAN, and select your locale settings. Then write the operating system to your SD card.‎

software_3

Once the software is written to the microSD card, remove the card from the PC and install it on the Pi. ‎Plug the SDR USB dongle into one of the Pi’s USB ports and power up the Pi.‎

Setup and Configure Your Flight Tracker

With your Pi booted, we need to connect to the Pi via SSH to install the flight tracker software. Note ‎that this can also be done locally on the Pi by connecting a keyboard, mouse, and monitor directly to ‎the Pi and opening a terminal window if you so choose.‎

Using a program such as PuTTY or Tera Term, open an SSH connection to your Pi using the hostname ‎you previously assigned, followed by “.local”. In my case, I can connect to my Pi at FR24Pi.local.‎

connect_4

name_5

Once logged in, make sure your Pi’s software is up to date by entering the following commands:‎

Copy Code
sudo apt update && sudo apt upgrade
sudo reboot

Allow your Pi to reboot, then reopen the SSH connection. The next command will install the ‎FlightRadar24 flight tracker software. If you haven’t already signed up for a free FlightRadar24 account, ‎you should go to https://www.flightradar24.com/premium/signup to do so now.‎

install_6

Install the flight tracker software:‎

Copy Code
sudo bash -c "$(wget -O - https://repo-feed.flightradar24.com/install_fr24_rpi.sh)"‎

Step 1.1: When prompted, enter the email address used for your FlightRadar24 account.‎

Fight Tradar24

Step 1.2: Since this is our first time setting up a flight tracker, we can leave this step blank.‎

blank_8

Step 1.3: MLAT is the process by which aircraft positional data is triangulated as was mentioned earlier. ‎To participate in these MLAT calculations, answer yes to this step.‎

yes_9

Step 3.A: Enter your antenna’s latitude. You can find the latitude, longitude, and elevation for your ‎location using this website: https://www.freemaptools.com/elevation-finder.htm

enter_10

Step 3.B: Enter your antenna’s longitude.‎

anntena_11

Step 3.C: Enter your antenna’s altitude. Remember to enter the altitude in feet.‎

altitude_12

You will then be asked to confirm these settings are correct.‎

settings_13

Step 4.1: Specify your receiver. For the RTL2832-based SDR USB dongle we are using, we can select ‎option 1.‎

receiver_14

Step 4.3: Leave this step blank.‎

step_15

Step 5.1 & Step 5.2: We don’t need these data feeds, so we can answer no to both.‎

no_16

Step 6: Enter 0 to disable logging.‎

logging_17

With that, the setup is complete, and we are now feeding flight data to FlightRadar24. Note that this ‎process may take some time to finish, so be patient and keep this window open until the command ‎prompt displays indicating the process is complete.‎

View Data

Now that setup is complete, you can view the flights your receiver is picking up by pointing your ‎browser to your Pi’s hostname followed by “/dump1090/gmap.html”. In my case, this information is ‎found at http://fr24pi.local/dump1090/gmap.html

view_18

Additionally, you can open the https://www.flightradar24.com/ homepage, select the filter option, ‎and input your radar ID from above to see only the aircraft your receiver is picking up.‎

homepage_19

homepage_20

Getting Better Reception

You will note from the above filter that we are not currently able to track many aircraft in our region. ‎This is due to the antenna being in a suboptimal location. Remember that antenna position matters, so ‎for better reception, try placing your receiver near a window or outside. In optimal conditions, you ‎may be able to track aircraft 250 miles from your receiver’s location. Below, you can see reception ‎and range improved dramatically when I relocated the receiver to its permanent position on one of my ‎outbuildings.‎

position_21

For the final placement, I mounted my Pi in a weatherproof enclosure with a clear lid so I can add a ‎camera as well, but that is for a different project. I drilled holes using a step drill bit and used cable ‎glands to seal the wires for the power supply and antenna to keep the enclosure weathertight so I ‎could mount my Pi outside where the antenna would have unobstructed access to aircraft ‎transmissions.‎

case_22

You may also notice I added a Fan SHIM to keep my Pi cool, for which you can find the installation ‎guide here: https://www.digikey.com/en/maker/projects/getting-started-with-fan-‎shim/314fa57086944d00871adb95ccf4a804

case_23

Going Further

FlightRadar24 is just one of many flight-tracking communities available. Should you decide, you would ‎like to feed your data to different or additional communities, the setup process is often similar and ‎requires no additional hardware. Here are a couple other flight tracker communities you may consider ‎contributing your data to:‎

https://www.adsbexchange.com/how-to-feed/#feedclient

https://flightaware.com/adsb/piaware/install

Référence fabricant SC0623
AC/DC WALL MNT ADAPTER 5.1V 13W
Raspberry Pi
Référence fabricant USDCOEM-32GB
MEM CRD MICSD 32GB 10UHS 1V10 3D
Delkin Devices, Inc.
Référence fabricant 1497
SOFTWARE DEFINED RADIO USB
Adafruit Industries LLC
Référence fabricant PTR-28483-C
BOX PLASTIC CLEAR 8.6"L X 6.3"W
Bud Industries
Référence fabricant PTX-18483-P
PLASTIC INTERNAL PANEL
Bud Industries
Référence fabricant 5308 905
CABLE GLAND 3-9MM 1/2" NPT
Altech Corporation
Référence fabricant 7211 486
NUT LOCKNUT PA NPT-1/2
Altech Corporation
Référence fabricant KTSB14
STEP DRILL BIT #14 - DOUBLE-FLUT
Klein Tools, Inc.
Référence fabricant PIM461
FAN SHIM FOR RASPBERRY PI
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.