New Product Discoveries - Omron's Motion Controller and STMicroelectronics' Dev System

DigiKey has always been the go-to for board level electronic components. Increasingly, however, we have started to support a wider breadth of Industrial Automation devices that are considered “finished goods products.” Today I want to introduce you to a couple different products with a focus on Industrial Automation.

The NX series from Omron are a set of PLC (Programmable Logic Controller) four axis motion controllers. In the 90s I used to work for a machine builder and it was quite difficult to generate sophisticated motion control. Problems such as having the ability to follow one axis to another and the ability to implement cam action from one PLC to another were very common. The Omron NX series have these functionalities built into the unit along with EtherCAT (Control Automation Technology). This allows for connectivity between units which means the one four axis control unit can actually control up to eight axes. This finished product is ready for implementation out of the box. Be sure to check out Scott Raeker’s “Omron NX1P2 Advanced Motion Controller” blog for more information on Omron PLCs.

On the other hand, for customers looking to build and develop their own machines, STMicroelectronics has the Nucleo development system. The Nucleo system is set up in such a way that you can stack the boards you want to utilize in your design to focus on what is important to you. In the case of a PLC, STMicroelectronics offers the X-NUCLEO-OUT01A1 Industrial Digital Output Extension Board. This board plugs directly onto the STM32 Nucleo, opening up options for high/low voltage and current IO along with wireless capabilities, essentially creating your own programmable logic controller. In addition, STMicroelectronics has implemented relay ladder logic, which allows your customers to make code changes on what is embedded on the microcontroller. Lindsay Foy has a great write up entitled “Creating Your Own PLC with STMicroelectronics”, about the Nucleo Industrial Digital Output Extension Board.

Specifically focused on the STMicroelectronics Nucleo platform, the article “Creating a Custom Wireless Programmable Logic Controller (PLC)” is available on the DigiKey website as a guide to developing your own wireless PLC.

Thanks for watching!

Achtergrondinformatie over deze auteur

Image of Randy Restle

Randall Restle heeft meer dan 40 jaar ervaring in de elektronische componentenindustrie. Hij is nu semi-gepensioneerd en heeft gediend als Vice President of Applications Engineering van DigiKey. Zijn ervaring omvat het aansturen van teams van bekwame applicatie-ingenieurs, technici en managementpersoneel om originele en unieke geavanceerde technologische producten te ontwikkelen.

Zijn persoonlijke bezigheden zijn onder andere digitale signaalverwerking, programmeerbare logica implementatie, verbeteringen in de motion control en software ontwerp. Hij is in het bezit van octrooien in verschillende industrieën en is een seniorlid van de IEEE. Randall behaalde BSEE-, MS- en MBA-diploma's aan de Universiteit van Cincinnati.

More posts by Randall Restle
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum