What You Need to Know About Pressure Sensors

Door Carolyn Mathas

Bijgedragen door Electronic Products


Used in applications spanning fluid/gas flow, speed, level and altitude, pressure sensors typically measure the pressure of gas or liquid within a specific environment. Pressure sensors act as transducers by generating a signal based on the degree of pressure that exists. They are frequently part of systems that monitor or control the gas or liquid being measured (Figure 1).

Fully integrated pressure sensor schematic

Figure 1: Fully integrated pressure sensor schematic.

Altitude pressure sensors are used in aircraft, satellites, weather, and barometric applications. Flow sensors are based on differential pressure measurements to measure liquid flow. Level- or depth-sensing applications include submarines, divers, and water towers. Leak sensors measure pressure decay.

Pressure sensor measurement falls into five categories:
  1. Absolute pressure is measured relative to a vacuum and the measurement is in pounds per square inch (PSI).
  2. Vacuum pressure is used to calculate pressure that is less than a given location’s atmospheric pressure.
  3. Gauge pressure measurement is relative to the ambient atmospheric pressure. Gauge pressure is stated in pounds per square inch gauge (PSIG).
  4. Differential pressure is measured relative to a specific reference pressure. The measurement is delivered in Pascals Differential (PAD) or in pounds per square inch differential (PSID).
  5. Sealed pressure sensors are calibrated by the manufacturer to measure pressure relative to sea level pressure.
When a pressure sensor delivers a voltage signal, the signal is converted to actual units of pressure. Conversion formulas vary based on the types of sensors used.

Many technologies span those used to manufacture pressure sensors, including semiconductor piezoresistive, strain gauge, microelectromechanical (MEMs), mechanical deflection, and vibrating capacitance.

Piezoelectric transducers

Force collector electronic pressure sensors typically use a force collector (diaphragm, bourdon tube, bellows, etc.) to measure strain due to pressure or force over a given area. They include piezoresistive strain gauges, capacitive, electromagnetic, piezoelectric, optical, and potentiometric sensors.

Piezoelectric (PE) pressure transducers use stacks of piezoelectric crystal or ceramic elements to convert motion to an electrical output—they need no external excitation. Because their output is very high impedance and their signal levels low, they require special signal conditioning. Often, PE transducers include an integral preamplifier so that output can be an amplified low output impedance signal. The integral amplifier requires external power from a constant-current supply, using the same two conductors as the signal circuit. The signal conditioner has a blocking capacitor to block the dc power supply voltage and to transmit an ac signal. Given that PE transducers are self-generating, dependent on changes of strain to generate electrical charge, they are not usable with dc or steady-state conditions.

Their distinct advantages are ruggedness and their usefulness at high temperatures.

Freescale’s MPX5999D piezoresistive transducer, for example, is a differential pressure sensor. It features an on-chip signal conditioning, temperature compensation, and calibration, and is designed for applications using a microcontroller or microprocessor with A/D inputs. The single-element transducer combines advanced micromachining, thin-film metallization, and bipolar semiconductor processing to provide accurate, high-level analog output signals proportional to applied pressure.

Barometric pressure sensing

The Bosch BMP085, in comparison, is a high-precision, ultra-low-power barometric pressure sensor (Figure 2). The sensor features ultra low power consumption down to 3 μA. Housed in a very small package, it is used for mobile applications requiring precise barometric pressure measurement such as GPS navigation enhancement, dead reckoning, in- and out-door navigation, leisure, sports and health monitoring, weather forecast, vertical velocity indication (rise/sink speed), and fan power control.

Bosch BMP085 digital, barometric pressure sensor

Figure 2: The Bosch BMP085 digital, barometric pressure sensor formula by which the absolute altitude is calculated from measured barometric pressure. (Courtesy of Bosch.)

Diaphragm-based sensors

Pressure sensing using diaphragm technology measures the pressure difference between two sides of a diaphragm. The Honeywell MLH Series all metal pressure sensors are examples (Figure 3). The MLH Series pressure sensor combines ASIC technology with a media-isolated metal diaphragm design. The sensor provides both value and performance for demanding applications. Fully temperature compensated, calibrated, and amplified, it is available in 50 to 8,000-psi ranges.

MLH Series by Honeywell

Figure 3: MLH Series by Honeywell are all-metal pressure sensors. (Source: Data Sheet)

Features include all-metal wetted parts for a variety of fluid applications; no internal elastomeric seals, which remove o-ring compatibility issues; amplified outputs, which eliminate the cost of external amplifiers; less than 2-ms response time for accurate high-speed measurement; and ratings of IP65 or better for protection in harsh environments.

The series is used in compressors, refrigeration and HVAC/R, industrial, hydraulics, medical, and transportation applications including braking and alternate fuels.

Advances and challenges

Recent advances in pressure sensors focus on miniaturization with integration of electronics and control capabilities into the same chip as the sensor resulting from the new, smaller form factors. The additional electronics result in performance gains, too. For example, improvements in high-vacuum gauges have resulted in extending ranges and an increase in “smart” capabilities. One application area that is opening up rapidly because of pressure sensor miniaturization is the medical segment. By reducing the size of the sensor for medical apps, low-pressure sensors are being used in external applications and invasive procedures.

The medical segment requires very low pressure (<5 psi) as well as improved linearity. The key is silicon micromachining to create a thin boss structure, etching the center boss to a thickness smaller than the substrate thickness, reducing the sensitivity of the device to gravitational force, achieving higher sensitivity within the device, and maintaining good linearity. With today’s new sensitive MEMS-based boss structures, it is possible to achieve pressure ranges down to 0.15 psi.

Among other advances, a skin-like sensor flexible enough for prosthetic limbs is being developed at Stanford University. The goal is to make touch-sensitive prosthetic limbs, pressure-sensitive badges, and more. Using a transparent film of carbon nanosprings that serve as electrodes, the sensor registers pressure. In this application, one layer stores electrical charge, acting in a manner similar to a battery. When pressure is exerted on the sensor, the layer compresses, altering the electrical charge it can store. This change is sensed by carbon nanotubes, prompting the sensor to transmit information regarding pressure levels.

Even though advances are frequent and research is active, pressure sensors are not without challenges. Common causes of pressure sensor failure include dynamic impact that results in sensor overload, spikes that cause a hole or tear in the diaphragm, moisture ingress whereby liquid seeps in through an interface and between a cable and the sensor, extreme temperature, stress when being calibrated, and wear and tear that produces drift and failure.

Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.

Achtergrondinformatie over deze auteur

Image of Carolyn Mathas

Carolyn Mathas

Carolyn Mathas draagt al meer dan 20 jaar redacteur-/schrijverhoeden bij publicaties als EDN, EE Times Designlines, Light Reading, Lightwave en Electronic Products. Ze levert ook aangepaste inhoud en marketingdiensten aan verschillende bedrijven.

Over deze uitgever

Electronic Products

Electronic Products magazine and ElectronicProducts.com serves engineers and engineering managers responsible for designing electronic equipment and systems.