Optimizing Remote IoT Networks: Advanced Integration of Advantech Connectivity Solutions with Taoglas Antennas
See how Advantech and Taoglas are teaming up to provide robust and uninterrupted connectivity solutions for IIoT applications.
Better Beer with IoT
See how the Internet of Things has helped micro-breweries produce more consistent and flavorful beers.
Gebruik een compacte 5G MIMO-antenne voor optimale connectiviteit en esthetiek
Publicatiedatum: 2024-06-19
Gebruik een compacte, laagprofiel 5G MIMO-antenne voor effectieve connectiviteit met behoud van toepassingsdiscretie en esthetiek.
How the Internet of Things (IoT) Is Used for Firefighting
As new IoT technology is being developed, it’s being incorporated into all aspects of emergency services to help keep first responders and the public safer.
Compact Multiband Patch Antenna Simplifies Design of RF Front-End for GNSS Receivers
Publicatiedatum: 2025-10-23
To handle multiple satellite constellation frequency bands, a GNSS receiver employs a multiband antenna to realize higher accuracy and reliability.
The compact planar inverted-F antenna (PIFA) is mechanically and electrically well-suited to compact, multiband devices such as smart phones and IoT nodes.
Choosing the appropriate antenna requires designers to consider the physical, electrical, and economical parameters that will best suit the application.
Antenna Polarization: What It Is and Why It Matters
Antenna polarization is an important factor in wireless-link performance; there are many options to consider when matching an antenna to the application.
An LTE Cat M1 modem provides a rapid development solution for low-cost, low-power, wide area IoT wireless applications.
Developers can create an IoT gateway simply by loading free firmware from Mozilla into a Raspberry Pi.
A hardware module and software package provide developers with a complete low-power solution to quickly implement Bluetooth mesh networking.