Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Image of Murata UltraBK™ MYTN Series of Power Modules - Transient Performance Transient

Transient performance with the company’s UltraBK™ MYTN series product is also significantly improved with this architecture given that the switching frequency of the system is running at 1MHz in 2-phase operation and with much less inductance in the system. This slide compares the transient response results against a leading COT mode module. Murata, in this instance, is using current mode control. However, Murata can achieve 25% better transient performance with half of the output capacitance than other available product options.

PTM Veröffentlicht am: