Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Image of Microchip's MCP6D11 Fully Differential Slide 2

A differential amplifier is unique in that it supports both differential inputs as well as differential outputs (as opposed to a single-ended output found on most operational amplifiers). In addition, the MCP6D11 offers a pin called VOCM that allows the output signal to be shifted by a DC value. For example this enables the output to match the range of an ADC. The MCP6D11 also features a power down pin, which allows the device to be placed in a low power mode when not in use.

PTM Veröffentlicht am: