Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
current-monitors-slide17

It can now be seen that the four required resistor values have all been calculated. All but RG are standard range resistor values. Even then, a value of 510Ω can be used if an error of 2% is okay or it can easily be made up of two 1k resistors in parallel.

PTM Veröffentlicht am: