Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
current-monitors-slide11

The two problems highlighted earlier are addressed by at least two devices in the ZXCT series. The ZXCT1010 has a separate ground pin which means the quiescent current is separated from the output. This practically removes a lower limit to how low the output current IOUT can be set. In addition, the ZXCT1020 provides for a programmable transconductance using a single external resistor. 

PTM Veröffentlicht am: