Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide5

This is a basic positive hot swap controller – the ADM4210.  The hot swap controller is used in conjunction with a number of components. The most significant being the sense resistor, MOSFET and timer capacitor. The sense resistor is used to measure the current on the main power path and is usually a very small resistance, in the order of milliohms. The N-Channel MOSFET is the main pass switch used to isolate the load, limit the current during a fault or during power-up, and, when fully enhanced, it will provide the main power for the module. The TIMER capacitor is critical to ensuring a maximum limit time is defined. When a fault occurs and the controller is limiting the current, the TIMER defines when to shutdown the MOSFET.

PTM Veröffentlicht am: