Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide14

This is an example of a SOA graph. The y-axis is the drain-source current, the x-axis is the drain-source voltage, and the dashed areas represent the amount of time the MOSFET can tolerate the power. Worst case conditions would be in the event of a short circuit where the entire load is across the MOSFET. First select the max voltage the system is operating under and draw a line up from the x-axis. Then select the current limit and draw a line from the y-axis and look at the intersection (8 or 9 ms in this example).

PTM Veröffentlicht am: