Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide13

Its important to highlight again the significance of the Safe Operating Area. The SOA is expressed by a graph in the MOSFETs datasheet which advises the user what combinations of load current and voltage drop are acceptable for what period of time. A MOSFET that cannot be maintained in this area will be destroyed or suffer significant damage. Therefore, a MOSFET should be chosen that will allow the time required to charge up the load in normal power up conditions and also still maintain SOA requirements.

PTM Veröffentlicht am: