Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Topic 3 Host System Overview Slide 11

This slide shows the host side RAM of the device. Concerto™ has 96 kB of RAM split into twelve distinct blocks of 8 kB each. Two additional 2 kB blocks are reserved for inter processor communication. M2C is for the M3 to control side exchange and C2M is for the C28x core to M3 exchange, C-blocks are dedicated to the M3 side; S blocks are shared. Initially TI will have all the eight shared RAM blocks matched to the M3 side. For control need, four by eight or 32kB might be needed. It is possible to remap S0, S2, S4, and S6 to the C28 side. Moving forward, if more is required, even the whole shared RAM, all of the blocks can be allocated to the DSP.

PTM Veröffentlicht am: