Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
powerSPIN Motor Control ICs Slide 9

From the control point of view, the number of power stages required to spin the motor in both clockwise and counter-clockwise directions is the main difference between the 3 types of Motors that PowerSPIN is suitable for. Depending on the kind of motor designed, various topologies exist, a DC motor requires an H bridge if bidirectional and half bridge if unidirectional, a BLDC motor, requires a three phase bridge, and a stepper motor requires a dual H-Bridge.

PTM Veröffentlicht am: