Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 8

The schematics shown on this slide illustrate how the MOS must be turned ON or OFF to perform the decay. When a slow decay occurs, the current recirculates in the high side or low side of the bridge. When a fast decay occurs, a large voltage is applied. A mixed decay is when both, slow and fast decay must be performed in the same time slot.

PTM Veröffentlicht am: