Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 7

To change the current level depends on the inductance and the voltage as the famous equation U= L * di/dt shows. That means, if the voltage is high, the change of current is fast, the energy in the coil is removed fast, it is a fast decay. Likewise, if the voltage is low, the change of current is slow, the energy is removed slowly, it is a slow decay.

PTM Veröffentlicht am: