Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
AC Switches Family - Part 1 Slide 17

Shown on this slide are some additional application examples. SCRs are commonly found in ignitors, ignitors in lighting control is called ballasts and inside high-intensity discharge ballasts to ignite the ballast. In the HID lamp, an ignitor is required to produce a high-voltage pulse. Typically an SCR can be used to generate the high-voltage pulse to ignite the lamp. In dimmers such as the wall dimmer in a house, Triacs are used to control the intensity of the light fixture.

PTM Veröffentlicht am: