Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Features of PicoLED Series

Shown here are ROHM Semiconductor’s standard lineup. ROHM has expanded the PICOLED colors to include fifteen colors, in addition, the PicoLED series has high reliability. By adopting a structure that prevents solder from getting inside the package, it is possible to dramatically reduce LED defects during soldering despite the thin form factor providing high reliability.

PTM Veröffentlicht am: