Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
topled
The customer will find the selection help for ams OSRAM's Midpower IR device Power TOPLED shown here. The bottom line displays the offer for 940 nm. Watch out for product designations with an “S“ after the numbers, because this means that one is dealing with a Nanostack at double voltages and almost double light output. Products including an orange cross have a version which is qualified with a test plan based on automotive grade standards. If the customer is making a design that is ultimately going to be used in an automotive application, one may want to focus on those products only.
PTM Veröffentlicht am: