Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Inrush-Slide3

ICL components are specially designed for effectively limiting excessive inrush currents when a device such as the STB is turned on. An ICL can handle this task because of its relatively high cold resistance, which initially absorbs these high currents. As a result of the current load, the device heats up and reduces its resistance by a factor of 10 to 50, and the power it draws reduces accordingly.

PTM Veröffentlicht am: