Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Inrush-Slide13

The EPCOS inrush current limiting product offering in the application of power supplies & compressor motor soft starting can be selected from our series of three different types the B57S153*, B57S235* or the B57S236* & are available in the resistance value range between 4.7 Ohms to 33.0 Ohms depending on the electrical circuit design.

PTM Veröffentlicht am: