Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Remote Control Infrared Receivers Slide 12

A common difficulty for manufacturers of consumer electronics is positioning the infrared receiver close to the receiving window and on the same plane as the circuit board. Holders can be used to raise the receiver above the circuit board or beyond its edge which allows the sensor to be placed directly behind the receiving window. Vishay helps manufacturers with this issue by offering the broadest portfolio of holders as well as the most options of bends and cuts in the industry.

PTM Veröffentlicht am:
PTM Updated on: 2015-02-26